Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! SPC5Studio - No such file or directory

Hi,I'm getting a lot of errors in SPC5Studio. If I use it with main.c without separating the library directory I'm working in, I don't have a problem. But when I want to separate the libraries, it doesn't work like an ordinary eclipse. Likewise, I do...

0693W00000DmXMSQA3.png

Resolved! Eeprom emulation problem in spc5660b

HiI have a serious problem with EEPROM emulationWriting and reading commands from EEPROM work well at first glance.When I read the ST documentation related to EEPROM "UM0558", I noticed one thing and that is "swaping". Swap should be done when block ...

Resolved! How to read out all CAN messages in the FIFO buffer

Hi,I'm new to the ST family of processorers and we are currentl using the SPC58EC discovery board at the company I'm currently working at.Background:I'm trying to make an application read out and print on serial what is being sent on the CAN bus. Rig...

adam_bm by Associate II
  • 9425 Views
  • 5 replies
  • 1 kudos

Resolved! How to move vector table in SPC560

HI All,We are using SPC560P controller in our project. I wrote bootloader to load main application from 0x00010000. Do I need to move vector table address for main application? How I can do it? Is there any examples are available to change the li...

Resolved! Why program loop in the function of irqSysHalt() ?

Hi, The program has been in irqSysHalt at the time of clock initialization, the clock initialization failed, but I don't know why? Has anyone encountered a similar problem?Program clock init fail:​The figure below is the clock configuration:​