2020-10-03 3:28 AM
i AM TRYING TO INSTALL PLS UDE uising the recommended link: http://spc5.drive.cloudforge.com/projects/spc5tools/updates
but all i can see is the following message.
Forbidden
You don't have permission to access /projects/spc5tools/updates on this server.
SPE 5 ide version 6.0
Similarly i am getting the above error.
Is some posts it was recommended to use UDE Visual Platform.
but i am unable to locate its directory.
Do we need to download UDE Visual Platform externally? is it a paid service?
Solved! Go to Solution.
2020-10-16 1:03 AM
Hello ,
Sorry i have missed the post ,
the 2 issues are PLS issues :
1) PLS UDE Plugin (32 bits) is not compliant anymore with SPC5Studio 6.0 (64 Bits)
(Delivery planned by PLS for Q1 2021)
You need to use PLS UDE External Tool directly.
There are a lot of posts on this subject
2) the button is disable because the installation of PLS UDE Tool Setup is not correct on Windows 10, Windows 7
(Default program for wsx file)
you can use the tool externally ..
I have submitted this ticket 3 years ago ... (link of the post) .. still no news...
you can use this tool to correct the default association of wsx file. (workspace pls)
https://community.st.com/s/global-search/PLS%20Default
Please ask to PLS
support@pls-mc.com
Best regards
Erwan
2020-10-03 11:12 AM
Execute and debug your application is not active
2020-10-03 3:38 PM
I am having same issues..
I also tried below method:
 
After bundle of software updates... Then it managed to install version 2.8 UDESTK...
However, another error...
2020-10-03 10:09 PM
hi,
@x7yu
I downloaded the UDE 5 EVAL from https://www.pls-mc.com/service/downloads/download-spc5-udestk/
I am trying to flash a simple led blink firmware
I tried to open debug.wsx
I am using AEK-MCU-C1MLIT1 development board.
Is there any setting we need to do in the SPC5 IDE
2020-10-16 12:09 AM
@VLELE.1
When you loaded the debugging file, it will show below windows to link up, then click ok. you should have your debugger works.
Actually I prefer to work on the debugger mode in SPC5 Studio, however I'm not managed to enable the button. If you success to do so?
 
2020-10-16 1:03 AM
Hello ,
Sorry i have missed the post ,
the 2 issues are PLS issues :
1) PLS UDE Plugin (32 bits) is not compliant anymore with SPC5Studio 6.0 (64 Bits)
(Delivery planned by PLS for Q1 2021)
You need to use PLS UDE External Tool directly.
There are a lot of posts on this subject
2) the button is disable because the installation of PLS UDE Tool Setup is not correct on Windows 10, Windows 7
(Default program for wsx file)
you can use the tool externally ..
I have submitted this ticket 3 years ago ... (link of the post) .. still no news...
you can use this tool to correct the default association of wsx file. (workspace pls)
https://community.st.com/s/global-search/PLS%20Default
Please ask to PLS
support@pls-mc.com
Best regards
Erwan
2021-03-04 10:53 PM
Hello,
I'm working with SPC5-UDESTK-EVAL USB/JTAG Adapter and I have the same problem with SPC5Studio debug. I tried install the SPC5Studio in Windows 7 (32 bits) but there isn't SPC5Studio 32 bits so What I can do?