Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

uC Hard reset occurs when put uC into Standby mode

Hello, i am Tuan from FPT.We are currently using SPC58EC for our project and the issue is HARD RESET occurs after we send request to put uC into Standby mode.It may work sometimes but usually reset uC. So do we have to check for any condition to make...

TNguy.47 by Associate
  • 781 Views
  • 0 replies
  • 0 kudos

Resolved! Application configuration

when i configure spc58nn project ,there is pineditor and clock tree ,the configurtion gui. and i cant find any other peripheral configuration gui,any one know this?

szhan.7 by Associate II
  • 4841 Views
  • 11 replies
  • 0 kudos

I2C Module doesn't figure out in Import sample with SPC58EC-DISP

I created my I2C test project, and click import samples from application library.Then, select SPC58EC-DISP, but there is no I2C Driver in Drivers tab.But, my colleague's SPC5 Studio figure out I2C Driver.What should I do to figure out I2C Driver?Atta...

DKim.34 by Associate
  • 2069 Views
  • 1 replies
  • 0 kudos

Resolved! I2C read is not working in latest spc5 studio 6.0, but the same code works in the old version spc5 studio. I don't know what to do.

Hello I'm sharan from yali mobilities. Here we are shifting from old spc5 studio to latest version spc5 studio 6.0. For testing I2C, I have used Arduino as a slave device. The programme which I have writen is attached as image. Arduino sends a ...

0693W00000NqYnDQAV.png
Ypvt .1 by Associate
  • 10016 Views
  • 14 replies
  • 0 kudos

Resolved! If I use SPC5 studio, do I need to be on a STM discovery kip or evaluation board to be able to flash and debug a board with a SPC582B or SPC584B MCU (I have also a probe SPC5-UDESTK) ?

Hi,I'm new in SPC5 world.I would like to use SPC5-Studio to start my project on a SPC582B product and I would like to be able to debug it.I have a probe SPC5-UDESTK that I have used to flash a project compiled with SPC5-Studio.It is not clear if I ne...

CCOLL.2 by Associate II
  • 3526 Views
  • 5 replies
  • 0 kudos

Writing DCF records in the code

Hello, I am using SPC58EC and I want to write DCF records, is it possible to do that in the code, I saw couple of example which are using Lauterbach script. If it is possible is there any application note or documentation for this? I also saw to upda...

0693W00000Nqq5dQAB.png
kb24 by Senior
  • 2392 Views
  • 2 replies
  • 0 kudos