Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

Resolved! L9663 driver code

ST engineer: HI. I am using PSI5 protocol by ST L9663 now。can you give me a driver code about L9663?

cfu.2 by Associate II
  • 2970 Views
  • 3 replies
  • 0 kudos

Resolved! Problem with FLEXPWM and eirq.

Hi,Can anyone advise or brief me how can i do the pwm using push button. I'm stuck with the output. So now my input is push button > eirqmy output is led > flexpwmMy problem now is the led not trigger everytime i press the button.It works on one time...

0693W00000Sv75iQAB.png
Angle by Associate II
  • 1454 Views
  • 2 replies
  • 0 kudos

Resolved! How do I accurately change the sample rate on the SPC560P?

My question is how to set the sample rate exactly? I know that I have to set it via the CTR register and there via the values INPCMP and INPSAMP. I also know where to set the values in the LLD-Config. However, I do not understand which change of the ...

TBles.1 by Associate II
  • 1756 Views
  • 1 replies
  • 0 kudos

Resolved! What will happened when changing a default values of INPSAMPLE, INPCMP, INPLATCH, OFFSHIFT in ADC of SPC560PXX? Then how to determine The values of these bitfields?

I tried setting up with default configuration parameters for ADC 1 on the SPC560PXX. However, it provides some random values. In the conversion timing register, I verified that INPSAMPLE's SPC560PXX default value is 5. When creating a Conversion grou...

0693W00000QKSuQQAX.png 0693W00000QKSv9QAH.png
VJ.4 by Associate
  • 1600 Views
  • 1 replies
  • 0 kudos

Resolved! How to SYNC PWM?

Hello, i have now this working code on SPC560P without sync flag. pwm_lld_start(&PWMD1, &pwm_config_pwm_cfg0); pwm_lld_start(&PWMD2, &pwm_config_pwm_cfg0); pwm_lld_start(&PWMD3, &pwm_config_pwm_cfg0); pwm_lld_start(&PWMD4, &pwm_config_...