Automotive MCUs

Ask questions and find answers on automotive microcontrollers like the SPC58 and their tools, such as the SPC5 Studio and how to implement JTAG unlocking.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to install your Root Certificate in StellarStudio JRE

When installing some StellarStudio  plugins http://*.srxstudio.org , you can meet the issue : sun.security.validator.ValidatorException: PKIX path building failed  It is typical IT Issue :face_screaming_in_fear:  in each corporate company. “"Path bui...

StellarStudio SR5E1 support is open to the mass market !

Dear all,   We are thrilled to announce that as of today, March 1st, 2024, SR5E1 device support in StellarStudio is available to the mass market !   This means that any user can effortlessly download the official StellarStudio installation packag...

preview.png

SPC58EC DISP not build aplications

I'm loading aplication's SPC58EC DISP, and debugging, but if I change the main.c this is the 9 problens. What it's, please?Another problem is that if I change and build the project, the changes not appearin the UDESTARTERKIT.

RPari.1 by Associate II
  • 1868 Views
  • 5 replies
  • 0 kudos

Resolved! What's the difference between c55_freegcc.a and c55_gcc.a

Good morning,I am developing a project for SPC574K2 with SPC5 studio V.6 which uses the C55 flash driver with ppc-freevle-eabi-gcc compiler. I suppose I need to use the c55_freegcc.a library, I would like to understand what is the difference from c55...

Resolved! SPC5 - functions, GTM, AutoDevKit, SPC754S

Im new into the SPC5-Studio. For the beginning it would help to have a document which shows me how to implement a Signal or sth else. For my 574s-Mcu there is just one example to let an led blink. IS there maybe a library of all Functions like toggle...

NDorn.1 by Associate II
  • 1409 Views
  • 1 replies
  • 0 kudos

Cannot flash using UDE STK 4.8

Hello,I have problems to flash a SPC5 MCU using UDE STK 4.8. I am using the PLS USB/JTAG Adapter for SPC5xxx. I have seen similar problems in this forum but I have tried different things during several hours and not solution has been reached.I am usi...

0693W000004I8KkQAK.png
MGuij.1 by Associate II
  • 2516 Views
  • 4 replies
  • 0 kudos

SPC5Studio 6.0-Asmiov and UDE Starter Kit 5.0 integration

Hi All,has anyone been able to get the inegration of UDE to work from within SPC5Studio (6.0)?the DEBUG button is grayed-out.Debug works fine from outside, but I would like to spawn it fro within the development IDE.I tried to install the extension b...

0693W000004Jw8lQAC.png
CoolMo by Associate III
  • 920 Views
  • 0 replies
  • 0 kudos

Resolved! Real time debugging with UDE STK

Hi,I am working on a SPC570S-DISP development board. I would like to know how to setup real time debugging of variables in the UDE STK software. I was able to add a variable to the Watch section. However, the value of the variable does not update. I...

NBula.1 by Associate III
  • 1183 Views
  • 1 replies
  • 1 kudos