2020-02-19 7:15 AM
Hi All,
We are using SPC560PL3 development board in our project. I'm facing issue with board reset, My code works for some time and resets. I tried to check with exceptions added handlers in the irq.c file. I have attached the file for reference, Please check.
When my board resets, I'm expecting some messages to print. But I'm not seeing any messages for reset issue.
My UART works fine.
Please let me know what I'm missing here. Do I need to set any option in the SPC5 studio? Or any code need to be modify to call these call back functions?
Help me to solve this issue.
Thanks,
Basava.
2020-02-26 5:33 AM
Hello ,
i recommend to use the debugger and check which IVOR you are going
check the PC,LR in assembler mode
Best Regards
Erwan
2020-05-08 3:36 AM
Depending on the version of the UART driver you are using, the sd_lld_write() requires interrupts to work
but if called in an interrupt handler, the interrupts are disabled, hence no data is sent out.
Update your SPC5Studio to the latest version which includes a serial driver able to recognize if called at interrupt time
and take the appropriate action in order to send data to serial port.