2022-05-02 7:07 AM
Hello,
I am using the STM32CubeProgrammer, version 2.10.0, and it does not detect the STM32L152VD-X reserved memory space, at address 0x0803000.
The STM32CubeProgrammer detects the correct device ID which is 0x437 but does not detect the correct device.
If I open the STM32_Prog_DB_0x437.xml file I see that the STM32L152VD-X is not even implemented.
This allows me to write to this reserved memory space which I believe is not a good idea
Questions:
2022-05-09 8:17 AM
Hi @Community member ,
This looks like the issue reported here.
@Houda GHABRI do you confirm this?
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-05-11 4:04 AM
Hi @Amel NASRI @Community member ,
It is a little bit different, the flash size is correct in this case : 384 KB.
And to ask your answers:
Please let me know if I missed something.
Houda
2022-05-11 4:10 AM
Hello @Amel NASRI @Houda GHABRI
I suppose that address between 0x08030000 and 0x08040000 is a reserved memory space for the STM32l151VD-X because this is what ST documentation says page 49 https://www.st.com/resource/en/datasheet/stm32l151vd-x.pdf
That why I am confused to why the CubeProgrammer allows to write that memory space without any warning. I also wonder what is the impact to writing to this address space since the cube allows it
2022-05-11 4:34 AM
Hi @Community member ,
Ok I see your point , thanks for bringing this up to our attention.
Currently this reserved area is not handled by CubeProgrammer, I will submit a request internally to fix this and handle the reserved area in future release.
Meanwhile user should take care to do not program on this address.
Houda