2020-01-17 01:44 AM
Hi,
I am experiencing a problem with STM32CubeProgrammer: it fails to program STM32L0s MCU when the size of the file to program is not a multiple of 8.
In the attached zip file, there are 2 .bin files containing 16 bytes of zeros (working.bin), and 20 bytes of zeros (failing.bin), respectively.
The first one can be programmed to the FLASH of an STM32L0 with STM32CubeProgrammer v2.3.0 without problem, but the second file fails with the following error :
10:32:42 : Memory Programming ...
10:32:42 : Opening and parsing file: failing.bin
10:32:42 : File : failing.bin
10:32:42 : Size : 20 Bytes
10:32:42 : Address : 0x08000000
10:32:42 : Erasing memory corresponding to segment 0:
10:32:43 : Erasing internal memory sector 0
10:32:43 : Download in Progress:
10:32:44 : Error: failed to download Segment[0]
10:32:44 : Error: failed to download the File
10:32:44 : Time elapsed during download operation: 00:00:01.648
Other possibly relevant information :
Thank you in advance for your help.
Olivier
2020-01-17 02:02 AM
Seem to recall similar issues being reported years ago on the HEX/DFU side, I posted a tool to fix it.
2020-01-17 02:28 AM
Hi @Community member
Thanks for your reply.
I guess a workaround is easy for .bin and .hex files, but a bit more complicated with .elf
Anyway, I wish ST can fix the problem, as it is quite annoying.
Olivier
2020-01-17 03:22 AM
Believe me, I can work with ELF/AXF files too.
ST has recurrent problems/issues with these types of thing, it exceeds my patience.
2020-01-17 03:24 AM
@Khouloud GARSI @Nawres GHARBI please can you flag this issue for review, thanks.
2020-01-17 03:32 AM
https://community.st.com/s/question/0D50X00009XkeovSAB/dfu-fail-verify-8-byte-align-magic
I just tend to code around issues as we need immediate resolution, blaming third-parties for missing shipping deadlines doesn't fly with the people I work with.
2020-01-17 04:21 AM
Thank you for providing sample files.
Ticket entered.
2020-01-17 06:51 AM
Thanks you all for your quick answers.
Hopefully ST will fix this soon, and I can work around it in the meantime.
2020-08-04 05:16 AM
FYI, this issue seems to have been fixed in STM32CubeProgrammer 2.5.0.