Hello,
When you're calling HAL_SPI_Transmit(), the chip is not ready to receive anything, so it is transmitting in the void.
and when you're calling HAL_SPI_Receive(), nobody is sending anything, so time out occurs.
So, maybe call HAL_SPI_Receive_IT...
Hello,
Please download the STM32F4x software package:
STM32F4 software package
There are 2 examples in STM32Cube_FW_F4_V1.28.0\Projects\STM324x9I_EVAL\Examples\CAN
Hope that helps.
Hello,
From what I can see, the fix is expected in software package version 1.7.0.
The current version available is 1.5.0.
I'm not able to tell when, as I don't have the planning.