STM32CubeProgrammer connection over UART error
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-03-09 6:33 AM
Hi, I've some problem using SMT32CubeProgrammer.
i am trying to connect via uart to micro stm32g491 but i receive some error messages.
15:21:34:034 : RTS low
15:21:34:034 : DTR low
15:21:34:171 : Serial Port COM15 is successfully opened.
15:21:34:172 : Port configuration: parity = even, baudrate = 115200, data-bit = 8, stop-bit = 1.0, flow-control = off
15:21:34:172 : No Init bits value is : 0
15:21:34:172 : Sending init command:
15:21:34:175 : byte 0x7F sent successfully to target
15:21:34:176 : Wait ends after 1 loop, dataready = 1, delay = 0
15:21:34:176 : Received response from target: 0x79
15:21:34:191 : Activating device: OK
15:21:34:192 : Sending GetID command and its XOR:
15:21:34:192 : byte 0x02 sent successfully to target
15:21:34:192 : byte 0xFD sent successfully to target
15:21:34:192 : Wait ends after 1 loop, dataready = 1, delay = 0
15:21:34:192 : Received response from target: 0x79
15:21:34:192 : Received 4 data bytes from target : 0x03047b7b
15:21:34:194 : Chip ID: 0x47B
15:21:34:195 : Sending Get command and its XOR:
15:21:34:195 : byte 0x00 sent successfully to target
15:21:34:195 : byte 0xFF sent successfully to target
15:21:34:195 : Wait ends after 1 loop, dataready = 1, delay = 0
15:21:34:195 : Received response from target: 0x7b
15:21:34:196 : Error: GET command not acknowledged!
15:21:34:197 : Reemission of Get command
15:21:34:197 : Sending Get command and its XOR:
15:21:34:197 : byte 0x00 sent successfully to target
15:21:34:214 : byte 0xFF sent successfully to target
15:21:34:214 : Received response from target: 0x1b
15:21:34:215 : Error: GET command not acknowledged!
15:21:34:218 : Reemission of Get command
15:21:34:218 : Sending Get command and its XOR:
15:21:34:222 : byte 0x00 sent successfully to target
15:21:34:224 : byte 0xFF sent successfully to target
15:21:34:226 : Received response from target: 0x33
15:21:34:228 : Error: GET command not acknowledged!
15:21:34:328 : UART PORT CLOSE
but if I try to communicate with the embedded bootloader of stm32 using another software (for example minicom or docklite) I can communicate correctly.
here are some messages on the serial:
09/03/2022 14:37:50.788 [TX] - 7F
09/03/2022 14:37:50.804 [RX] - 79
09/03/2022 14:37:51.966 [TX] - 02 FD
09/03/2022 14:37:51.971 [RX] - 7A 03 04 7B 3F 79
09/03/2022 14:37:53.091 [TX] - 01 FE
09/03/2022 14:37:53.094 [RX] - 79 33 00 00 7B 3F
09/03/2022 14:37:53.787 [TX] - 02 FD
09/03/2022 14:37:53.793 [RX] - 7B 3F 03 04 7B 7B 3F
09/03/2022 14:37:54.490 [TX] - 01 FE
09/03/2022 14:37:54.497 [RX] - 79 71 00 00 7B 3F
why can't i use stm32cubeprogrammer software?
Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-03-15 6:42 AM
Hi @ERazz.3 ,
I tested with the same device you have (same Device ID and Bootloader version), it works fine on ST Board with both CubeProgrammer 2.9.0 and 2.10 version.
So I suspect a wiring issue , you can try to reduce the Baudrate and test again?
Houda
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-03-09 6:53 AM
Hi @ERazz.3 ,
Are you using the last CubeProgrammer version 2.10.0.? If not can you please switch to this version which contain many enhancement related to UART connection?
Houda
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-03-09 7:20 AM
i've installed stm32cubeprogrammer 2.10.0.
it seem to be the same...
here the log.
14:29:04:255 : Activating device: OK
14:29:04:256 : Board : --
14:29:04:256 : Sending GetID command and its XOR:
14:29:04:257 : byte 0x02 sent successfully to target
14:29:04:260 : byte 0xFD sent successfully to target
14:29:04:260 : Wait ends after 1 loop, dataready = 1, delay = 0
14:29:04:306 : Received response from target: 0x79
14:29:04:306 : Received 4 data bytes from target : 0x01047b79
14:29:04:307 : Chip ID: 0x47B
14:29:04:307 : Sending Get command and its XOR:
14:29:04:309 : byte 0x00 sent successfully to target
14:29:04:312 : byte 0xFF sent successfully to target
14:29:04:312 : Wait ends after 1 loop, dataready = 1, delay = 0
14:29:04:312 : Received response from target: 0x6f
14:29:04:313 : Error: GET command not acknowledged!
14:29:04:313 : Reemission of Get command
14:29:04:313 : Sending Get command and its XOR:
14:29:04:314 : byte 0x00 sent successfully to target
14:29:04:316 : byte 0xFF sent successfully to target
14:29:04:316 : Received response from target: 0x61
14:29:04:316 : Error: GET command not acknowledged!
14:29:04:317 : Reemission of Get command
14:29:04:317 : Sending Get command and its XOR:
14:29:04:317 : byte 0x00 sent successfully to target
14:29:04:317 : byte 0xFF sent successfully to target
14:29:04:318 : Received response from target: 0xee
14:29:04:318 : Error: GET command not acknowledged!
14:29:04:341 : UART PORT CLOSE
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-03-09 7:35 AM
Hi @ERazz.3 ,
Ok I will check , can you tell me if you are using CLI or GUI? If CLI command line used please.
Houda
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-03-09 7:52 AM
@Houda GHABRI i'm using GUI.
Thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-03-15 3:51 AM
Hi @ERazz.3 ,
I did same checks using NUCLEO-G491RE board and connection via UART works correctly.
I see in your traces that the Device ID is not correct :
14:29:04:306 : Received 4 data bytes from target : 0x01047b79
14:29:04:307 : Chip ID: 0x47B
The correct device ID for STM32G491 is 0x479 so tell me please if you are using an ST Board? Also send me please the Bootloader version of your chip ( value of Bootloader is in 0x1FFF6FFE address).
Houda
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-03-15 6:04 AM
Hi @ERazz.3
The Baudrate value used during connection please?
Houda
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-03-15 6:24 AM
Hi, at address 0x1FFF6FFE I see 0xD2.
we're using our custom bord.
thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-03-15 6:27 AM
Hi, 155200
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2022-03-15 6:42 AM
Hi @ERazz.3 ,
I tested with the same device you have (same Device ID and Bootloader version), it works fine on ST Board with both CubeProgrammer 2.9.0 and 2.10 version.
So I suspect a wiring issue , you can try to reduce the Baudrate and test again?
Houda