User Activity

Hi, I've some problem using SMT32CubeProgrammer. i am trying to connect via uart to micro stm32g491 but i receive some error messages. 15:21:34:034 : RTS low 15:21:34:034 : DTR low 15:21:34:171 : Serial Port COM15 is successfully opened. 15:21:34:172...
hi, i'm using a STM32G491 and i can't use embedded bootloader over UART1. i'v set BOOT_LOCK(bit) to 0, Boot0(pin) to 1, nBoot1(bit) to 1 ans nBoot_SW(bit) to 1. when i try to connect the mcu to STCubeProgrammer over UART i receive this message error:...