2022-03-01 2:41 PM
I just installed the CubeProgrammer and I'm following the Populate the target and boot the image guide. When I get to section 1.1.1.1.2.6 Populate the SDCard and click "Connect" I get this error:
But if I execute this on the command line:
sudo /opt/st/stm32cubeprgrammer_2.9.0/bin/STM32_Programmer_CLI -c port=usb1 -w flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsvEverything works perfectly fine. I get this:
Is anyone familiar with that error on the GUI? If it works on the CLI it should work on the GUI too, isn't it?
Solved! Go to Solution.
2022-03-11 7:23 AM
Hi @m4l490n ,
Sorry for the delay.
It seems that binary path is not filled with correct path, that's why CubeProgrammer still searching for an old path.
You need to give the path of binaries used as shown in screenshot below :
Can you please try and tell me if the issue is resolved?
Houda
2022-03-01 5:30 PM
Is there a reason you're running it in superuser mode? Are you also running the GUI in superuser mode?
Linux support on ST tools isn't awesome. Looks like it's not looking in the right folder. Unlikely that databases are stored in /home/.
2022-03-02 4:31 AM
Hi @MM.10alagon ,
Can you please clarify the exact steps you are making to launch the GUI ?
Is it from command line or from the Desktop shortcut ?
Did you moved or modified the default CubePrg directory structure ?
Houda
2022-03-02 11:52 AM
I have to run it as superuser because if I don't, then neither the CLI nor the GUI can see the USB.
Yeah, that database is not stored at /home that is where I'm starting the GUI. So, it seems that I need to go to <install dir>/bin every time I need to run it? Isn't adding the bin directory to the PATH supposed to avoid this?
2022-03-02 11:55 AM
I have to launch the GUI from the command line with sudo, otherwise, it won't see the USB port.
I just realized that if I go to <install_dir>/bin and run the GUI (<install_dir>/bin $ sudo ./STM32CubeProgrammer) from there then I don't get that error.
But now it is complaining about not finding the file I'm choosing. I don't know why it is changing the path. It says there in the blue message that is read the file
/home/mmalagon/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Starter-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/images/stm32mp1/flashlayout_st-image-weston/trusted/FlashLayout_sdcard_stm32mp157c-dk2-trusted.tsvSo I don't know why it is complaining about not finding this file:
Error: File does not exist: /home/mmalagon/STM32MPU_workspace/STM32MP15-Ecosystem-v3.1.0/Starter-Package/stm32mp1-openstlinux-5.10-dunfell-mp1-21-11-17/images/stm32mp1/flashlayout_st-image-weston/trusted/arm-trusted-firmware/tf-a-stm32mp157c-dk2-usb.stm32Why is it trying to use that file, that is not the one I have specified.
2022-03-11 7:23 AM
Hi @m4l490n ,
Sorry for the delay.
It seems that binary path is not filled with correct path, that's why CubeProgrammer still searching for an old path.
You need to give the path of binaries used as shown in screenshot below :
Can you please try and tell me if the issue is resolved?
Houda
2022-03-14 3:53 PM
@Houda GHABRI Thanks for helping.
Yes, correcting the path solves the issue. Now it works ok.
I still have the issue of having to open STM32CubeProgrammer from the CLI as sudo. Opening it using the app launcher icon doesn't work. Do you know why is this?
This is a little bit cumbersome because to make the cubeprogrammer work I have to go to <install_dir>/bin and then execute it as sudo. Isn't the icon supposed to open the application in a usable state? Or what am I missing?
2022-03-15 2:01 AM
Hi @MM.10alagon ,
Glad to know that path issue is fixed.
For the app launcher icon I confirm there was issue but should be fixed in last CubeProgrammer version 2.10.0, can you please test and tell me if it is OK?
Houda