2023-03-01 01:42 AM
I tried to use an ST-LINK V2 on macos Monterey but it does not work:
However, as an USB device it is available:
I also tried running the programmer with sudo.
I have confirmed that this ST-LINK works on a Windows machine.
I use STM32CubeProgrammer v2.13.0 with ST-LINK V2-1.
Do you have any idea?
2023-03-01 01:58 AM
I installed the v2.10.0 and sometimes it works but it does not. So, the issue is still there.