Debug issue
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-09-01 12:42 AM
Hello,
I have an issue debug issue in my custom board. The debug session works for a while and then stop to working and suddenly after many tries it works again.
When the debug session doesn't work, I get:
STMicroelectronics ST-LINK GDB server. Version 5.9.1
Copyright (c) 2021, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
LogFile Name : C:\Users\***\Debug\st-link_gdbserver_log.txt
Logging Level : 31
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
COM frequency = 4000 kHz
Target connection mode: Attach
Reading ROM table for AP 0 @0xe00fffd0
Hardware watchpoint supported by the target
ST-LINK Firmware version : V2J38M27
Device ID: 0x418
PC: 0x78f9e0
ST-LINK device status: RUN_MODE
ST-LINK detects target voltage = 3.26 V
ST-LINK device status: RUN_MODE
ST-LINK device initialization OK
Waiting for debugger connection...
Waiting for connection on port 61234...
Waiting for connection on port 61235...
Accepted connection on port 61234...
Debugger connected
Try halt...
ST-LINK device status: HALT_MODE
Enter STM32_HardwareReset() function
STM32_HardwareReset(), failure reset target.
ST-LINK device status: RESET_MODE
------ Switching to STM32CubeProgrammer -----
-------------------------------------------------------------------
STM32CubeProgrammer v2.8.0
-------------------------------------------------------------------
Log output file: C:\Users\***\AppData\Local\Temp\STM32CubeProgrammer_a14944.log
ST-LINK SN : 0668FF343537424257252146
ST-LINK FW : V2J38M27
Board : NUCLEO-F302R8
Voltage : 3.25V
Error: ST-LINK error (DEV_TARGET_CMD_ERR)
Encountered Error when opening C:\ST\STM32CubeIDE_1.4.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.0.202105311346\tools\bin\STM32_Programmer_CLI.exe
------ Switching context -----
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
Stopping port 61235
Received stop for port 61235, not accepting new connections.
I use ST-LINK device and pins SWCLK, SWDIO and NRST are connected to the custom board MCU STM32F105VC. (of course 3.3v and GND).
The debug configuration is attached.
Thank you.
- Labels:
-
DEBUG
-
STM32CubeProgrammer
-
STM32F3 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-09-03 3:01 AM
Could be that the MCU goes to deep sleep mode? Because I can program the MCU and suddenly it stopped. Doesn't ST-LINK bring the MCU out off sleep mode?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-09-03 8:40 AM
I write this in first reply. And basic is when you plan use debug you cant use SWD pins in code usw.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2021-09-03 8:53 AM
Pins and attached flip-flops, etc are generally non-functional when unpowered..
There may be some DBGMCU related settings to keep certain domains and clocks enabled, but generally the processor is going to dump debug connectivity when entering SLEEP or STANDBY states. Frequently LSI is also in a domain that powers down. The manuals should provide specificity.
When doing "debugging" of power or transitional states it is better perhaps to use a serial port for telemetry/diagnostics so you can squawk as you enter and leave low power states. Among other things this is *significantly less invasive*, and more reflective of operation in the field.
Up vote any posts that you find helpful, it shows what's working..

- « Previous
-
- 1
- 2
- Next »