2024-09-21 11:06 PM - last edited on 2024-09-23 8:09 AM by mƎALLEm
I am in work with a product firmware with STM32G030k8 with additional EEPROM M24C04 I coudlnt ble to instal the driver files .
Is this the righ tway am doing,can any one please address this?I am not able to hightlight or install Thanks.
Solved! Go to Solution.
2024-09-25 4:46 AM
OK.
Could you please uninstall the old version (you didn't mention the version you have) and download/install the latest version: 6.12.1?
2024-09-23 8:08 AM
Hello @meena ,
You need to check one of the available drivers:
For example, for M24 / M24XX, check the box on the right and click OK.
In "Middleware and Software Packs" menu , click on X-Cube-EEPRMA1 and check the box "Board Part EEPROM"
After generating the code, M24XX driver is included in the project.
Attached an example of ioc file.
Hope it helps.
2024-09-25 3:41 AM
Hi Thanks yes but for some reason I am not able to tick (enable )the driver or install.May I know what is wrong
2024-09-25 3:48 AM
Sorry, I didn't understand. Did you try the ioc file I provided ?
I'm able to open the EEPROM driver
Which driver you are not able to open:
2024-09-25 3:59 AM
havent got a solution for this .I couldnt able to download the packs For some reason Iam not able to instal the particular board part.I am using stm32G030k8 MCU
2024-09-25 4:02 AM
Please describe exactly the behavior. What do you mean by:
@meena wrote:
.I couldnt able to download the packs For some reason
The download couldn't start?
2024-09-25 4:04 AM
I am trying to install the drivers for M24 EEPROM chip which is interfaced with STM32G030k8 MCU.
As you said I have tried but my issue is I am not able to check that part or if i click install its nothing happening
2024-09-25 4:12 AM - edited 2024-09-25 4:18 AM
Do you mean you cannot check that blue box?
Or when you click on Install button nothing happens?
2024-09-25 4:18 AM
Can you please tell me whether the EEPROM M24c02-R below can be used with STM32G030K8
2024-09-25 4:20 AM - edited 2024-09-25 4:21 AM
@meena wrote:
Can you please tell me whether the EEPROM M24c02-R below can be used with STM32G030K8
Did you open the ioc file I've attached previously? it's based on STM32G030K8.