cancel
Showing results for 
Search instead for 
Did you mean: 

Would you like to help us with issue with regards on WiFi_HTTP_Server?

IGuer
Associate

We are developing an application based on Wi-Fi connectivity. For that purpose, we took your example: “WiFi_HTTP_Server�? from “STM32Cube_FW_L4_V1.13.0�?. We are using   B-L475E-IOT with SW4STM32.

The application can control the LED, but after 3 or 4 time to try to change the LED, the page stops. No more loads after reset the board.

We tried on two boards B-L475E-IOT with the same result.

3 REPLIES 3

Hi @IGuer​ ,

Thanks for the feedback,

It will be fixed next CubeMX release.

Regards,

Nesrine

Cvega.11
Associate II

Hello my friend

Do you know how to use the wifi module (ISM43340-M4G-L44-10 CF) of the stm32h7b3i-dk board?

How to configure a from baud to AT command ISM43340-M4G-L44-10 CF?

Any example of a WIFI http server with stm32h7b3i-dk ???

Cvega.11
Associate II

the same happens to me

manage to correct the problem ??