2025-02-17 12:47 PM - last edited on 2025-12-26 5:56 AM by ELABI.1
"Hello, I am opening a new project in STM32 Cube IDE. When I create the project, the main .c files are not being generated. During the process, it gives the error shown below. When I try to log in with my email address and password to download the required package, the program closes the page but does not connect. How can I solve this issue?"
2025-02-18 8:21 AM
Hello @Haydar5988
Are you using any proxy to connect? If it's the case check this article on how to configure the network settings for STM32CubeIDE and STM32CubeMX : How to set the network connection parameters for S... - STMicroelectronics Community
Also, the article describes how you can install FW packs manually without connecting.
KR,
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.