2019-06-12 10:44 AM
We are developing an application based on Wi-Fi connectivity. For that purpose, we took your example: “WiFi_HTTP_Server�? from “STM32Cube_FW_L4_V1.13.0�?. We are using B-L475E-IOT with SW4STM32.
The application can control the LED, but after 3 or 4 time to try to change the LED, the page stops. No more loads after reset the board.
We tried on two boards B-L475E-IOT with the same result.
2019-07-09 02:07 AM
Hi @IGuer ,
Thanks for the feedback,
It will be fixed next CubeMX release.
Regards,
Nesrine
2020-09-06 02:46 AM
Hello my friend
Do you know how to use the wifi module (ISM43340-M4G-L44-10 CF) of the stm32h7b3i-dk board?
How to configure a from baud to AT command ISM43340-M4G-L44-10 CF?
Any example of a WIFI http server with stm32h7b3i-dk ???
2020-10-03 11:47 PM
the same happens to me
manage to correct the problem ??