2025-02-17 8:05 AM
I made a change to my project (using an STM32H7S3L8 part), saved the results, and a few days later tried to reload the project, but got a "Not a valid ioc file" error message. Here is the output of the log file:
```
2025-02-17 10:59:38,352 [FATAL] ProjectFactory:568 - Exception caught
java.lang.NumberFormatException: For input string: ""
at java.lang.NumberFormatException.forInputString(NumberFormatException.java:67) ~[?:?]
at java.lang.Long.parseLong(Long.java:719) ~[?:?]
at java.lang.Long.valueOf(Long.java:1157) ~[?:?]
at com.st.microxplorer.mcu.memorymap.MemInfoExtractor$ETHInfoExtractor.onETHEnable(MemInfoExtractor.java:4561) ~[STM32CubeMX:?]
at com.st.microxplorer.mcu.memorymap.MemInfoExtractor.completInit(MemInfoExtractor.java:252) ~[STM32CubeMX:?]
at com.st.microxplorer.mcu.memorymap.MemoryMapService.MMTActivated(MemoryMapService.java:1259) ~[STM32CubeMX:?]
at com.st.microxplorer.mcu.memorymap.MemoryMapService.loadConfigV3(MemoryMapService.java:2578) ~[STM32CubeMX:?]
at com.st.microxplorer.mcu.Mcu.loadConfProperties(Mcu.java:6750) ~[STM32CubeMX:?]
at com.st.microxplorer.mxsystem.ProjectFactory.swingWorkerLoad(ProjectFactory.java:494) ~[STM32CubeMX:?]
at com.st.microxplorer.util.ProcessBarDialog.performAction(ProcessBarDialog.java:86) ~[STM32CubeMX:?]
at com.st.microxplorer.util.ProcessBarDialog$1.doInBackground(ProcessBarDialog.java:157) ~[STM32CubeMX:?]
at com.st.microxplorer.util.ProcessBarDialog$1.doInBackground(ProcessBarDialog.java:154) ~[STM32CubeMX:?]
at javax.swing.SwingWorker$1.call(SwingWorker.java:305) ~[?:?]
at java.util.concurrent.FutureTask.run(FutureTask.java:317) ~[?:?]
at javax.swing.SwingWorker.run(SwingWorker.java:342) ~[?:?]
at java.util.concurrent.ThreadPoolExecutor.runWorker(ThreadPoolExecutor.java:1144) ~[?:?]
at java.util.concurrent.ThreadPoolExecutor$Worker.run(ThreadPoolExecutor.java:642) ~[?:?]
at java.lang.Thread.run(Thread.java:1583) ~[?:?]
```
It would be rather useful to tell me which key had the problem so that I could edit the file in vim (at least enough to bring the tool up). (This is independent of the tool writing a file that it later could not read, but I don't have the information on which change that I made that tickled that bug.) This issue is occurring on CubeMX v6.13.0.
Solved! Go to Solution.
2025-02-18 12:39 AM
Hello @sf
Actually, this is a known issue with the STM32CubeMX 6.13 version which occurs when activating the memory mapping tool (MMT) and Ethernet.
As a temporary workaround, you can open the IOC by following these steps:
- Open the IOC file with a text editor
- Delete all references to "MMTAppReg"
- Modify "MMTAppRegionsCount" to "MMTAppRegionsCount=0"
- Reopen the IOC file with STM32CubeMX 6.13.0
KR,
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-02-17 2:58 PM
> at com.st.microxplorer.mcu.memorymap.MemInfoExtractor$ETHInfoExtractor.onETHEnable(
This hints to something related to ETH.
Generally, if something worked before and makes trouble now - use your version control (git or whatever) and roll back to happiness.
2025-02-17 4:02 PM
Yes, that was obvious. Unfortunately, the number of lines changed were quite numerous -- to the point that I'm abandoning CubeMX as the tool.
2025-02-18 12:39 AM
Hello @sf
Actually, this is a known issue with the STM32CubeMX 6.13 version which occurs when activating the memory mapping tool (MMT) and Ethernet.
As a temporary workaround, you can open the IOC by following these steps:
- Open the IOC file with a text editor
- Delete all references to "MMTAppReg"
- Modify "MMTAppRegionsCount" to "MMTAppRegionsCount=0"
- Reopen the IOC file with STM32CubeMX 6.13.0
KR,
Souhaib
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.