cancel
Showing results for 
Search instead for 
Did you mean: 

Using the IDE Version: 1.0.2 Build: 3566_20190716-0927 (UTC) 'DMA continuous request' entry stays in DISABLED condition, no way to set it to ENABLED

WBayo
Associate II

Circular buffer DMA is defined for an ADC.

I want it to start and continue to convert forever.

If I manually correct the init procedure which was generated, that works well

5 REPLIES 5
Amel NASRI
ST Employee

which device are you using?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

WBayo
Associate II

STM32F446

Amel NASRI
ST Employee

Hi @WBayo​ ,

This seems to be the same issue as DMA Continuous Requests - Not selectable option on STM32F446RE Nucleo Board.

@Nesrine.JLASSI​ : could you please have a look to both discussions?

Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

WBayo
Associate II

Yes, indeed.

It is just what I did to go around the bug in the IDE.

I am now using the version   STM32CubeMX 5.3.0.201907110903

and the bug is still not corrected.

​Hello @WBayo​ 

Thanks for the feedback, the problem is known, it will be corrected in the next STM32CubeMX release.

Best regards,

Nesrine