2021-12-07 2:49 AM
The image shows my clock configuration for the STM32F469IIT. I want a 12MHz output from MCO2 and I found that I could theoretically achieve this using the PLLI2SCLK input. However, when I use this configuration, the device is not recognised by the PC via USB. I have also measured the signal using a scope and I seem to get a frequency of 6MHz. I can increase the clock speed on MCO2 to be "24MHz" and this will produce a 12MHz signal.
I won't post any code just yet as this issue may be more fundamental, but let me know if more information is needed. I hope someone can explain why this doesn't work.
I'm using an external 8MHz clock, USB FS but I am not using the I2S peripheral itself, only the clock divider and multiplexer.
Solved! Go to Solution.
2021-12-10 12:12 AM
Hi @C.East2 ,
This issue is confirmed and an internal ticket (ID 119067) is submitted in order to fix this in the coming release of CubeMx.
(PS: Internal ticket ID 119067, this is an internal tracking number and is not accessible or usable by customers).
Thank you again for having reported the point.
Imen
2021-12-07 3:58 AM
Hello,
can you check your HSE crystal is really 8 MHz? Is USB working when you set your PLL parameters for 4 MHz HSE crystal?
From your description and verification using MCO this looks possible.
2021-12-07 4:08 AM
Hi @Lubos KOUDELKA ,
HSE crystal is definitely 8MHz.
When I select the MCO2 source to HSE, I get 8MHz. I can also use the division to achieve the correct values.
2021-12-07 4:37 AM
@Lubos KOUDELKA
I've found that MX is wanting to enable the HSI in the SystemClock_Config (See image below). When I remove 'RCC_OSCILLATORTYPE_HSI' the device works. However, every time I regenerate code from MX, it appears. I can't (from the clock config diagram) where I am enabling/using the HSI. I am using the LSI for the RTC.
2021-12-07 6:19 AM
Yes, I just tried on my side and I can also see problem with RCC_OSCILLATORTYPE_HSI in init, I will report to our developers. Unfortunately now I don't have any easy solution for to skip RCC_OSCILLATORTYPE_HSI after STM32CubeMX re-generation, you will need to do it manually.
2021-12-07 6:26 AM
Thanks @Lubos KOUDELKA ,
For the time being I can assign HSI to the MCO1. This means it's being used and will not cause an error. It also means I don't have to keep deleting the code after generation. Hopefully a fix can be made.
2021-12-08 1:40 AM
Hello @C.East2,
Thank you for having reported this issue.
Hi @Lubos KOUDELKA Thank you for bringing this post to my attention.
I added CubeMX team @Khouloud OTHMAN @Khouloud ZEMMELI in this post to review this issue.
Thanks
Imen
2021-12-10 12:12 AM
Hi @C.East2 ,
This issue is confirmed and an internal ticket (ID 119067) is submitted in order to fix this in the coming release of CubeMx.
(PS: Internal ticket ID 119067, this is an internal tracking number and is not accessible or usable by customers).
Thank you again for having reported the point.
Imen