2021-10-19 8:27 AM
I am using CubeIde for the first time.
First test - run minimal program with HAL from CubeIDe Configurator, under debugger
Simple program, only SYSTICK and uart , but SysTick_Handler() is not trigged at all .
And function HAL_Delay hangs because uwTick is always 0. Tried with setting brakepoint inside handler - no results
Used HSI, SYSCLK 16MHZ, Cortex System Timer 16MHz,
RCC GPIO and USART1 - HAL configured.
here is main() generated from cubeide (I removed comments):
-----------------------------------------------------------
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_USART1_UART_Init();
HAL_Delay(100);
// here program hangs, when reaches HAL_Delay function. uwTick = 0
while (1)
{
}
}
-----------------------------------------------------------
and here is the SysTick_handler from stm32g0xx_it.c
-----------------------------------------------------------
void SysTick_Handler(void)
{
HAL_IncTick();
}
-----------------------------------------------------------
2024-11-19 12:55 PM
Hi!
Please look at this post: https://community.st.com/t5/stm32cubemx-mcus/systick-handler-not-called-stm32g0b1/m-p/744998/highlight/true#M30159
(It's one post before yours.)