cancel
Showing results for 
Search instead for 
Did you mean: 

SysTick_Handler not called, STM32G0B1

Xme
Associate II

I am using CubeIde for the first time.

First test - run minimal program with HAL from CubeIDe Configurator, under debugger

Simple program, only SYSTICK and uart , but SysTick_Handler() is not trigged at all .

And function HAL_Delay hangs because uwTick is always 0. Tried with setting brakepoint inside handler - no results

Used HSI, SYSCLK 16MHZ, Cortex System Timer 16MHz,

RCC GPIO and USART1 - HAL configured.

here is main() generated from cubeide (I removed comments):

-----------------------------------------------------------

int main(void)

{

  HAL_Init();

 SystemClock_Config();

 MX_GPIO_Init();

 MX_USART1_UART_Init();

 HAL_Delay(100);

// here program hangs, when reaches HAL_Delay function. uwTick = 0

 while (1)

 {

 }

}

-----------------------------------------------------------

and here is the SysTick_handler from stm32g0xx_it.c

-----------------------------------------------------------

void SysTick_Handler(void)

{

 HAL_IncTick();

}

-----------------------------------------------------------

20 REPLIES 20