2022-08-12 2:27 PM
Hello.
I have stm32h743vit6. After Cubemx 6.3.0, the adc clock prescaler setting is not available, it does not appear. Also, even if I open the adc channels, the adc mux is never active on the Clock Config page.
In older projects (6.3.0 and earlier) adc clock settings can be configured. Is this an error?
Solved! Go to Solution.
2022-12-28 3:50 AM
Hello @AUNAL.1 ,
This issue is fixed in STM32CubeMX 6.7.0.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-08-12 5:43 PM
Check the code and the structures.
Review the Reference Manual and Errata.
2022-08-13 9:24 AM
I am creating a new project. There is no written code.
Cubemx is malfunctioning while generating the adc code because the adc clock presaler option is not available. The fact that the clock presacler setting is not available is the main cause of the error. Try it and see.
2022-12-28 3:50 AM
Hello @AUNAL.1 ,
This issue is fixed in STM32CubeMX 6.7.0.
When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.
Thank you.
Kaouthar
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.