2017-12-21 5:44 AM
I am wroking on a project using two microcontrollers a STM32F412 and a STM32L011 (8K flash, 2k RAM) .The STM32L011 is used as RTC to manage the power comsumption of the STM32F412.
I used STM32CubeMx to generate the code to set the peripherics that I use within the L011 (I2C, RTC, RCC). The problem is the size of the generated code once compiled is bigger than the 8k available inside the flash of the L011.
I only compile the genretaded code without writting a line of code.!
How could be possible to get a bigger code than the place to stored it for a defined STM32?
I think I did something wrong but I can find what is wrong.
Someone could provide me any ideas to resolve this situation. (i can not change the micro)
You will find in attachment the .ioc file. The genrated code from STM32Cube Mx is trasnfered on a Eclipse platform
and is used GNU ARM tools.
.Thanks in advance for your help
Best regards
Serge LOPEZ
#stm32cubemx #stm32l0xx #program-size2017-12-22 9:03 AM
Try the following gcc options:
-Os -ffunction-sections -fdata-sections -Wl, - gc-sections
2017-12-22 10:15 AM
My code
Without the above options:
text 51500 data 1140 bss 2640
flash : 56736 ( 86.57 %)ram : 3780 ( 46.14 %)With the above options:
text 14236 data 1124 bss 2568flash : 19456 ( 29.69 %)ram : 3692 ( 45.07 %)With the above options plus -flto:
text 11136 data 1128 bss 2700flash : 16360 ( 24.96 %)ram : 3828 ( 46.73 %)2018-01-08 6:33 AM
Hello Rosiney,
Thanks for answering me.
I checked the compile commande that I used and these options are already declared.
FY, the compile cmd used is :
'
arm-none-eabi-g++ -mcpu=cortex-m0plus -mthumb -Os -fmessage-length=0 -fsigned-char -ffunction-sections -fdata-sections -ffreestanding -flto -Wunused -Wuninitialized -Wall -Wextra -Wmissing-declarations -Wconversion -Wpointer-arith -Wpadded -Wshadow -Wlogical-op -Waggregate-return -Wfloat-equal -g -T mem.ld -T libs.ld -T sections.ld -nostartfiles -Xlinker --gc-sections -L../ldscripts -Wl,-Map,L011.map --specs=nano.specs -o L011.elf 'src\\_write.o' 'src\\main.o' 'src\\stm32l0xx_hal_msp.o' 'src\\stm32l0xx_it.o' 'system\\src\\clib\\_cxx.o' 'system\\src\\clib\\_exit.o' 'system\\src\\clib\\_sbrk.o' 'system\\src\\clib\\_startup.o' 'system\\src\\clib\\_syscalls.o' 'system\\src\\clib\\assert.o' 'system\\src\\cmsis\\startup_stm32l011xx.o' 'system\\src\\cmsis\\system_stm32l0xx.o' 'system\\src\\cortexm\\_initialize_hardware.o' 'system\\src\\cortexm\\_reset_hardware.o' 'system\\src\\cortexm\\exception_handlers.o' 'system\\src\\diag\\Trace.o' 'system\\src\\diag\\trace_impl.o' 'system\\src\\stm32l0xx\\stm32l0xx_hal.o' 'system\\src\\stm32l0xx\\stm32l0xx_hal_cortex.o' 'system\\src\\stm32l0xx\\stm32l0xx_hal_dma.o' 'system\\src\\stm32l0xx\\stm32l0xx_hal_flash.o' 'system\\src\\stm32l0xx\\stm32l0xx_hal_flash_ex.o' 'system\\src\\stm32l0xx\\stm32l0xx_hal_flash_ramfunc.o' 'system\\src\\stm32l0xx\\stm32l0xx_hal_gpio.o' 'system\\src\\stm32l0xx\\stm32l0xx_hal_i2c.o' 'system\\src\\stm32l0xx\\stm32l0xx_hal_i2c_ex.o' 'system\\src\\stm32l0xx\\stm32l0xx_hal_pwr.o' 'system\\src\\stm32l0xx\\stm32l0xx_hal_pwr_ex.o' 'system\\src\\stm32l0xx\\stm32l0xx_hal_rcc.o' 'system\\src\\stm32l0xx\\stm32l0xx_hal_rcc_ex.o' 'system\\src\\stm32l0xx\\stm32l0xx_hal_rtc.o' 'system\\src\\stm32l0xx\\stm32l0xx_hal_rtc_ex.o' 'system\\src\\stm32l0xx\\stm32l0xx_hal_tim.o' 'system\\src\\stm32l0xx\\stm32l0xx_hal_tim_ex.o'
'
I
Kind regards
p.s.: All the best for 2018 !
2018-01-08 10:59 AM
I compiled with makefile but had to change 'STM32L011D3Px_FLASH.ld':
_Min_Heap_Size = 0x100; /* required amount of heap */
_Min_Stack_Size = 0x200; /* required amount of stack */Make: 4.2.1
GCC: (arm-none-eabi) 6.3.1 Size after: text data bss dec hex filename 5440 1088 948 7476 1d34 build/release/bin/test_l0/test_l0.elf ________________ Attachments : L011.rar : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hy0r&d=%2Fa%2F0X0000000b4g%2Flj4NueqALk2QW74e9EZTjK2eGdimhpXeOwpc5HTys0E&asPdf=false2018-01-11 12:34 AM
If your code optimization possibilities have been exhausted, I see two options.
Problems like yours happen much more often than you might think ...
2018-01-11 1:07 AM
I did not find the file STM32L011D3Px_FLASH.ld
What I found is the fololowing file mem.ld. Heap size and stack size are defined through equation with other parameters. So I was no confident to change them. I just was able to upgrade _Minn_Heap_Size that 's it.
________________ Attachments : mem.ld.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyCR&d=%2Fa%2F0X0000000b4V%2FTy7mx_vNCs7BhZ1SrDuvNBKQXQ_MUDlAkccbLAD5vwc&asPdf=false2018-01-11 2:05 AM
Cube LL drivers is another way to go... I work with small flash a lot and switched to LL
2018-01-11 2:06 AM
Hello,
Indeed using Cube HAL for STM32 MCUs with small size of Flash could be problematic, because most or all (like in this example) Flash can be consumed by generated code and there is small or no space for user code.
This limitation was a reason why ST introduced some time ago so called Low Layer (LL) libraries. This is an alternative solution to HAL libraries. Thanks to it developers can create applications based on working out of the box API for MCU's resources, but additionaly they benefit from significantly reduced code size. Both HAL and LL are supported by STM32CubeMX and user selects for each peripheral separately HAL or LL. In order to make such configuration inside STM32CubeMX please click in main menu Project -> Settings and in opened window select Advanced Settings tab.
I believe this solution will allow you to fit in MCU's Flash size and still you will be able to use STM32CubeMX and ST libraries (LL) for your application development.
Regards
Szymon2018-01-11 2:28 AM
AvaTar wrote:
Problems like yours happen much more often than you might think ...
Indeed - 'sizing' the microcontroller for the task at hand is a key skill.
Premature optimisation is a root of many evils.
8K flash is very small!
You need to examine the Map file to see what is using all the space.
You can also use nm:
https://sourceware.org/binutils/docs/binutils/nm.html
You're not using floating-point maths, are you ... ?
(and beware that Cube/HAL isn't sneaking it in through the back door)