cancel
Showing results for 
Search instead for 
Did you mean: 

USBX Mutex does not work - CubeMX code generator BUG

matt-crc
Senior III

Hello, I'm trying to implement a USBX host... and the code generates a lot of runtime errors.  I assume everything is setup properly from CubeMX, but the code always fails. 

mattcrc_3-1741165785810.png

 

1- I see that the mutex was created from the debug session: (ux_system_mutex)

mattcrc_0-1741162907896.png

2- the system fails when trying to initialize the UX system.

mattcrc_1-1741163003693.png

3- The error came from _ux_utility_mutex_on() and generates an error code 0x04

VOID  _ux_utility_mutex_on(UX_MUTEX *mutex)
{

UINT    status;

    /* Call ThreadX to get system mutex.  */
    status =  tx_mutex_get(mutex, TX_WAIT_FOREVER);

    /* Check for status.  */
    if (status != UX_SUCCESS)
    {

        /* Error trap. */
        _ux_system_error_handler(UX_SYSTEM_LEVEL_THREAD, UX_SYSTEM_CONTEXT_UTILITY, status);
    }

    /* Return to caller.  */
    return;
}

so, it is trying to get the mutex (ux_system_mutex) and then wait forever....

4- If I look at the AzRTOS manual: 0x04

mattcrc_2-1741163342925.png

5- The base code was auto generated by CubeMX.  So basically it is trying to initialize memory using a mutex before starting the threads....

6- to make matters worse, the error code (status) is not passed to the calling function properly, so it took a lot of time to find this problem, and the ux_error_handlers does absolutely nothing (ie no while(1))

 

1 ACCEPTED SOLUTION

Accepted Solutions
FBL
ST Employee

Hi @matt-crc @a.gajdacs 

Regarding the mutex operation is being called before threadX scheduler has started.

I got the confirmation, you need to avoid initializing USBX stack before starting the ThreadX. This is a known limitation in USBX.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL

View solution in original post

7 REPLIES 7
FBL
ST Employee

Hi  @matt-crc 

Would you attach ioc file to reproduce?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL
matt-crc
Senior III

Hi @FBL 

see attached

Matthew

 

Hi @FBL 

This is my first project with STM32, so I'm not too familiar on how ST works... so I have 3 questions:

1- How long does it usually take for ST to analyze and fix the problems reported (weeks, months, etc)? and how often do you release updates?

2- Do you know of a way to disable the auto-code generator from updating a particular file? (for example if I fix this problem in app_azure_rtos.c, I don't want CubeMx to update this file anymore.)

3- It would be really nice if CubeMX always added a user area at the very beginning of the file and a user area at the end of the file to all generated files, then users can disable the updating of a file. This would fix item #2 above.  Can this be done for all your files? (example shown below)

/*User code begin - start of file */
/*User code end - start of file */
----
CubeMX code will be updated in this area
----
/* User code begin - end of file */
/* User code end - end of file */

 then our code would look like this:

/*User code begin - start of file */
#ifdef (USE_CUBEMX_CODE)
/*User code end - start of file */
----
CubeMX code will be updated in this area
----
/* User code begin - end of file */
#endif
----
User code will remain untouched here - for bug fixes and enhancements
----
/* User code end - end of file */

Hi @matt-crc 

An internal ticket is submitted to dedicated team to fix initialization order in app_azure_rtos.c (204777)
Another ticket is submitted to Tools team to add user section at the end of app_azure_rtos.c file to make it more customizable (204781).

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL

Hi,

Any news on this matter? It's been 4 months, and I still see this bug in action. In fact, it has been reported like a year ago. https://community.st.com/t5/stm32cubemx-mcus/usbx-blocking-isr/td-p/698199

FBL
ST Employee

Hi @matt-crc @a.gajdacs 

Regarding the mutex operation is being called before threadX scheduler has started.

I got the confirmation, you need to avoid initializing USBX stack before starting the ThreadX. This is a known limitation in USBX.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL
matt-crc
Senior III

Hi @FBL 

you're too funny... I guess you should inform your programmers because the base code was from your examples.  Since it was 6 months ago, I don't remember which USBX H7 it was from, but I'm pretty sure they all do it.

Matt