2024-07-01 09:53 AM - edited 2024-07-01 10:17 AM
We are pleased to announce you that the official release of STM32CubeMX V6.12.0 is available.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-07-01 12:34 PM
Why does it still show that the latest version is 6.11 here???
2024-07-01 01:13 PM - edited 2024-07-02 04:33 AM
> Please refer to the wiki under this link and the release note RN0094.
the link is broken. now fixed.
> Add support new CPNs STM32G4: Add support STM32G4 'Z’ and STM32G414
Which one is it???
2024-07-02 01:54 AM - edited 2024-07-02 02:03 AM
Sorry wrong forum...
Padawan
And again
Jumping around the files after Debug.
Again: Opening a ticket and promising to resolve it "asap" is not a solution!
What a poor performance after several years.
Padawan
2024-07-02 02:03 AM
Hello @BarryWhit
First let me thank you for posting.
Support new CPNs (Commercial Part Number )STM32G4
STM32G473xx
STM32G414xx
Thx
Ghofrane
2024-07-02 04:33 AM
Oh, so none of them were right? hillarious. Thank you.
2024-07-05 01:45 AM
Hi,
µC: STM32G070RBTx
after updating to 6.12.0, the code generator shows an error with the ADC configuration.
If I reset the configuration and start over, as soon as I set the Sequencer to "Not Fully Configurable", the error occurs:
Regards,
Edwin
2024-07-05 02:09 AM
Hello @EdwinID
First let me thank you for reporting.
This issue has been raised to our dev team (internal ticket 185851).
THX
Ghofrane
2024-07-05 10:50 AM
Hi,
What does the "OEM Restricted" Marketing Status of the new STM32G414x mean?
Ari
2024-08-08 07:43 PM
6.12 crashes when opening an existing 6.11.1 project on Linux Debian Jessie (8). Works OK on Ubuntu Jammy Jellyfish (22.04).
Exception in thread "AWT-EventQueue-0" java.lang.NullPointerException: Cannot invoke "com.teamdev.jxbrowser.browser.Browser.mainFrame()" because "this.browser" is null
Full backtrace attached
Updating the project file using 6.12 on the Ubuntu system and now the project reads OK.
BTW: Good to see that the syscall & sysmem generation bugs have been fixed
ALSO: Trying to attach a file called 'bug' results in an error of 'filetype .bug not supported' . You do realise I hope that not all files have a filename extension and if it does it may not be 3 characters!!