Skip to main content
Associate II
August 30, 2024
Question

Incompatibility between X-CUBE-TOUCHGFX and X-CUBE-GNSS

  • August 30, 2024
  • 1 reply
  • 1229 views

Hello dear community,

I'm using a STM32U5A9J-DK.

I want to start in CubeMX a project based on this board, X-CUBE-TOUCHGFX and X-CUBE-GNSS softwares.

However, CubeMX warns me (in the "Software Packs Component Selector") that theses are incompatibles between them.

For example, if I choose X-CUBE-GNSS first then try to choose TouchGFX, it tells "This component cannot be selected: this application cannot be selected while the application from pack STMicrolectronics.X-CUBE-GNSS1.6.0.0 is selected":

PascalP_0-1725018811809.png

and vice versa.

I guess that is because the touch screen use PI6 (DSI_BL_CTRL) pin that can be used as reset pin or wake up pin for GNSS: is this correct ?

Is there a way to "force" or bypass this recommendation ?

Thanks a lot in advance for your help

 

This topic has been closed for replies.

1 reply

ST Technical Moderator
September 3, 2024

Hello @PascalP 

Thank you for bringing this issue to our attention, I will check it internally and get back to you as soon as possible.

KR,

Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.