cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX 5.1.0 released

Nawres GHARBI
ST Employee

Dear community

We are pleased to announce the release of STM32CubeMX v5.1.0

What’s new ?

 

  • Performance enhancements for improved user experience.
  • Font size is now customizable (Click "Window" -> "Font size")
  • User interface updates
  • Graphics updates: TrueSTUDIO® is supported by TouchGFX Designer.

  • Added the support of the first MPU: STM32MP1 Series.
    • New devices: STM32MP151xx, STM32MP153xx, and STM32MP157xx.
    • New boards: STM32MP157A-EV1, STM32MP157C-EV1 and STM32MP157C-DK2
    • Features: Tj versus Ta calculation for PCC, DDR Test Suite, Device Tree generation, etc.
  • Added the support of the STM32WB Series:
  • New devices: STM32WB55xx.
    • Examples in MX format available in the STM32Cube_FW_WB_1.0.0 STM32CubeWB MCU Package.
    • Features: PCC Bluetooth® Low Energy feature.
  • Added the support of USBPD Middleware for G0 Series

Supported STM32Cube package versions:

·          STM32F0 V1.9.0

·          STM32F1 V1.7.0

·          STM32F2 V1.7.0

·          STM32F3 V1.10.0

·          STM32F4 V1.24.0

·          STM32F7 V1.15.0

·          STM32G0 V1.1.0

·          STM32H7 V1.3.2

·          STM32L0 V1.11.0

·          STM32L1 V1.8.1

·          STM32L4 V1.13.0

·          STM32MP1 V1.0.0

·          STM32WB V1.0.0

Main Fixed issues

 

  • 46874 [MX-Clock] include frac formulas in frequency calculation when PLL frac is enabled.
  • 51206 [MX-TIM] Break filter to be removed for TIM15, 16 and 17.
  • 53264 [MX-Pinout][STM32H750IBKx] G10 must be VSS and not VDD.
  • 55690 [MX-Board] Wrong configuration of special PHY reg for STM32F746 Discovery.
  • 56760 RCC for LTDC clock of STM32L4R9.
  • 56828 [MX-ETH]PHY DP83848 should support also RMII mode.
  • 56999 FreeRTOS™ initialization sequence.
  • 57348 [MX-LWIP] Exception generated due to undefined parameter in the ftl.
  • 57520 [MX-SPI] Missing Alternate Function Open Drain in SPI configuration mode.
  • 58043 [MX-TouchSensing] Missing user label in function MyTKeys_ErrorStateProcess().

Known limitations

Please read the Release note for the known limitations

https://www.st.com/resource/en/release_note/dm00107607.pdf

30 REPLIES 30

@Nawres GHARBI​ How do we access the bug tracker where the details of the CubeMX fixed and outstanding issues are explained?

Nawres, I suspect there might be something wrong with the package for MacOS

  1. CubeMX builtin "Check for Updates" doesn't detect an update from 5.0.1
  2. So I downloaded it from the website and extracted the zip. There is a Windows EXE for running CubeMX, but nothing for installing, so I can't even use the "java -jar" workaround from the doc file.

@Nawres GHARBI​ It would be great if you would post these announcements AFTER the stuff is actually available on the web site (unless you intend to annoy your customers ;-)

anio1491
Associate II

Hello,

I was able to update my CubeMX (finally) to the release today (v5.1.0), but I am not able to update the L0 firmware package to the lastest version. I can see that there is a new packet available, but the download fails, and therefore, I cannot generate anymore code.

Any idea on what's wrong?

Please see screenshots attached.

Regards,

Andreea

0690X000006DpUMQA0.png

0690X000006DpURQA0.png

When I setup PWM or OC clocks for example I did setup the main clock in Clube MX 50 Mhz

I used 50 divider to get 1 MHz instead I was getting something like 490 KHz. They were pretty close but never close. Like the main oscillator was not accurate.

When I did 25 divider I got like 990 KHz. I do have oscilloscope connected to the pins so I can see what is coming out.

I cannot see doing any mistake all looks simple and straightforward in Cube MX

But still if I do 50 MHz in Cube Mx shouldn't I get

RCC_OscInitStruct.PLL.PLLN = 50;

instead of

RCC_OscInitStruct.PLL.PLLN = 25;

Joerg Wagner
Senior III

Can we trust RC6 or should I wait for a final release?

could you please attach the used ioc

Hi @Dave Nadler​ 

The bug tracker isn't accessible for the moment but it is planned to be in the future

Hi @Dave Nadler​ 

The package was available on the web site when the post has been published, it may sometimes have a little late to appear to you depending on the web synchronization

Hi @Joerg Wagner​ 

The RC6 is the final release for 5.1.0