cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX 5.0.1: LPUART1 missing NVIC menu

Gökhan Taşçı
Associate

I migrate my CubeMx project that is based on stm32l072cbtx to version 5.0.1 but in connectivity menu, LPUART1 NVIC settings doesn't appear. So I can't enable LPUART1 interrupts with code generation. Is there any problem? or I've missed something

0690X000006DiEMQA0.jpg

1 ACCEPTED SOLUTION

Accepted Solutions

Hi @Gökhan Taşçı​ 

Thanks for the feedback.

You are right, i was able to reproduce the issue and it will be fixed in the next STM32CubeMX release.

Best Regards,

Nesrine.

View solution in original post

3 REPLIES 3

Hi @Gökhan Taşçı​ 

Thanks for the feedback.

You are right, i was able to reproduce the issue and it will be fixed in the next STM32CubeMX release.

Best Regards,

Nesrine.

Hi @Nesrine.JLASSI​ ,

I have updated the CubeMX to the latest version (v 5.1.0) and the issue is still there. I cannot enable the LPUART interrupt.

Any ideas?

Regards,

Andreea

​Hi @anio1491​ 

Thanks for the feedback.

It will be available soon.

Ragards,

Nesrine