Skip to main content
Associate III
January 17, 2025
Question

CubeMX setting incorrect baudrate for STM32WL33CC LPUART

  • January 17, 2025
  • 5 replies
  • 1247 views

Hi All,

1. [Part Number] STM32WL33CC1
2. [Environment] Windows OS, STM32CubeIDE version 1.17.0, Firmware package STM32Cube FW_WL3 V1.0.0
3. [Schematics] STM32 Nucleo-64 development board
4. [Details] See below.
5. [Expected behavior] Data sent at 115200 from a remote terminal should be received by the STM32WL33 using the same baudrate
6. [How to reproduce] Build the LPUART_TwoBoards_ComIT example by ST and connect terminal program and set baudrate to 115200. 
7. [Occurrence] Consistent
8. [Sanity checks] What are the checks that you have already performed (example: Have you reviewed the existing examples - GitHub, Cube...).

Details

I imported an old UART driver from a previous project that I had successfully used for many years on STM32 microcontrollers. However, I noticed it wasn’t functioning as expected on the STM32WL33. Specifically, when I sent a command from Tera-Term, the received data on the STM32WL33 appeared corrupted, as if a different baud rate was being used.

To clarify, I’m not concerned with the low-power features of the STM32WL33’s LPUART. My project requires two UARTs, so I decided to use LPUART1 as the second COM port.

I’m running the system using an HSE clock at 48 MHz.

After performing basic sanity checks, I suspected the issue might stem from my inexperience with the LPUART. To investigate further, I decided to test the LPUART functionality using one of ST’s example projects, specifically the LPUART_TwoBoards_ComIT example.

Following the example instructions, I flashed two boards: one as a transmitter (Tx) and the other as a receiver (Rx). The two devices successfully communicated with each other. However, when I connected a logic analyzer to observe the data transmission at 115200 baud, I found that the data was garbled. Surprisingly, both boards appeared to accept the transferred data without issue.

Using the logic analyzer, I measured a bit width of 13 µs, corresponding to a baud rate of approximately 76923.077—significantly different from the expected 115200 baud. When I set the logic analyzer to 76923, I could correctly interpret the transmitted data.

This led me to debug the driver in-depth, where I eventually identified the root of the problem in the stm32wl3x_hal_rcc_ex.c file.

 

uint32_t HAL_RCCEx_GetPeriphCLKFreq(uint32_t PeriphClk)
{
 uint32_t frequency, spiFreqValue, krmValue;

 /* Check the parameters */
 assert_param(IS_RCC_PERIPHCLOCK(PeriphClk));

 /* No if clausule is covered */
 frequency = 0;

 switch (PeriphClk)
 {
 //
	 // Ohter code removed for brevity
	 //
#if defined(RCC_CFGR_LPUCLKSEL)
 case RCC_PERIPHCLK_LPUART1 :
 switch (__HAL_RCC_GET_LPUART1_CLK_CONFIG())
 {
 case RCC_LPUART1_CLKSOURCE_LSE:
 frequency = LSE_VALUE;
 break;
 case RCC_LPUART1_CLKSOURCE_16M:
 frequency = 16000000;
 break;
 default:
 frequency = HSE_VALUE / 2;
 break;
 }
 break;
#endif /* RCC_CFGR_LPUCLKSEL */
 default :
 break;
 }
 return (frequency);
}

 

The case RCC_LPUART1_CLKSOURCE_16M was missing setting the frequency as well as a break statement so it was automatically going to the default case. Adding the following line

 

frequency = 16000000U;
break;

 

Seem to have solve the problem. Unfortunately every time I change the ioc file. This gets overwritten by the default code with the bug so I thought to notify ST in order to see if the fix can be incorporate in the new build of the IDE and/or if there is a work around that can be suggested

Ola

This topic has been closed for replies.

5 replies

STTwo-32
ST Technical Moderator
February 4, 2025

Hello @ola 

First, are you using the example or your own code. If so, Could you please share more about that.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
olaAuthor
Associate III
February 4, 2025

Hi STTwo-32

Thank you for your reply.


First, are you using the example or your own code. If so, Could you please share more about that.

 

 No I am not using my own example. In my original post I wrote I am using ST LPUART_TwoBoards_ComIT example

Regards

Ola

STTwo-32
ST Technical Moderator
February 4, 2025

Hello @ola 

Thank you so much for reporting this behavior. I've escalated to the concerned team for correction on the coming releases (under internal ticket number 202227).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
April 1, 2025

Thank you very much,

I encountered this problem in the project of stm32wl33kc. I used STM32Cube FW_WL3 V1.1.0. Unfortunately, this problem was not fixed synchronously.

At first I was suspicious of the hardware, testing the hardware and removing electrical interference, didn't look too far into the HAL library, and then I searched online and found your description.

 

 

C:\Users\Administrator\STM32Cube\Repository\STM32Cube_FW_WL3_V1.1.0\Drivers\STM32WL3x_HAL_Driver\Src\stm32wl3x_hal_rcc_ex.c

Then I modified the file directly to avoid generating code overrides each time.

Associate III
May 28, 2025

This fix will work, provided that the HSE divider is 3. It should be returning either HSE/3 or HSE/4, depending on the CLKROOTDIV value, which is not taken into account here.