2022-04-18 10:24 AM
Hello,
I'm using StmCubeMX 6.5.0 with StmCubeIDE 1,9.0.
I'm trying to set up ADC1 channel 7 (PA2 pin) in polling mode on STM32U585QII device.
HAL_ADC_GetValue is always returning 0 while it should return something else.
Below is a simple main function:
int main(void)
{
/* USER CODE BEGIN 1 */
uint32_t adc_value;
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* Configure the System Power */
SystemPower_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_ADC1_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
if(HAL_ADC_Start(&hadc1) == HAL_OK)
{
HAL_ADC_PollForConversion(&hadc1, 100);
adc_value = HAL_ADC_GetValue(&hadc1);
}
HAL_Delay (200);
}
/* USER CODE END 3 */
}
Here is also system clock configuration:
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Supply configuration update enable
*/
HAL_PWREx_ConfigSupply(PWR_LDO_SUPPLY);
/** Configure the main internal regulator output voltage
*/
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE0);
while(!__HAL_PWR_GET_FLAG(PWR_FLAG_VOSRDY)) {}
/** Macro to configure the PLL clock source
*/
__HAL_RCC_PLL_PLLSOURCE_CONFIG(RCC_PLLSOURCE_HSE);
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_BYPASS;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
RCC_OscInitStruct.PLL.PLLM = 1;
RCC_OscInitStruct.PLL.PLLN = 62;
RCC_OscInitStruct.PLL.PLLP = 1;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 2;
RCC_OscInitStruct.PLL.PLLRGE = RCC_PLL1VCIRANGE_3;
RCC_OscInitStruct.PLL.PLLVCOSEL = RCC_PLL1VCOWIDE;
RCC_OscInitStruct.PLL.PLLFRACN = 4096;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2
|RCC_CLOCKTYPE_D3PCLK1|RCC_CLOCKTYPE_D1PCLK1;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.SYSCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB3CLKDivider = RCC_APB3_DIV2;
RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV2;
RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{
Error_Handler();
}
}
I also tried capturing with interrupt (HAL_ADC_Start_IT) but is also returning value 0.
There is voltage on VDDA pin.
What I'm doing wrong or what clould be causing this problem?
Best regards,
Miha
Solved! Go to Solution.
2022-05-11 06:41 AM
Below code needs to be added after inicialization of adc in order for adc to work:
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWREx_EnableVddA();
2022-04-18 11:35 PM
In the repository, you will find an example for the ADC.
\Repository\STM32Cube_FW_U5_V1.1.0\Projects\NUCLEO-U575ZI-Q\Examples\ADC\ADC_SingleConversion_TriggerSW_IT\Src
/* Perform ADC calibration */
if (HAL_ADCEx_Calibration_Start(&hadc1, ADC_CALIB_OFFSET, ADC_SINGLE_ENDED) != HAL_OK)
{
/* Calibration Error */
Error_Handler();
}
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* Start ADC group regular conversion */
if (HAL_ADC_Start_IT(&hadc1) != HAL_OK)
{
/* Error: ADC conversion start could not be performed */
Error_Handler();
}
2022-04-19 12:18 PM
@victagayun I have added calibration as mentioned in example and it did not help. Now it stucks in function: HAL_ADCEx_Calibration_Start -> LL_ADC_IsCalibrationOnGoing. Calibration does not end.
I have also enabled ICACHE and it also did not help.
2022-04-19 03:51 PM
Can you check versus this?
ADC_ChannelConfTypeDef sConfig;
HAL_Init();
/* Configure the system clock to 400 MHz */
SystemClock_Config();
/*##-1- Configure the ADC peripheral #######################################*/
AdcHandle.Instance = ADCx;
if (HAL_ADC_DeInit(&AdcHandle) != HAL_OK)
{
/* ADC de-initialization Error */
Error_Handler();
}
AdcHandle.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV2; /* Asynchronous clock mode, input ADC clock divided by 2*/
AdcHandle.Init.Resolution = ADC_RESOLUTION_16B; /* 16-bit resolution for converted data */
AdcHandle.Init.ScanConvMode = DISABLE; /* Sequencer disabled (ADC conversion on only 1 channel: channel set on rank 1) */
AdcHandle.Init.EOCSelection = ADC_EOC_SINGLE_CONV; /* EOC flag picked-up to indicate conversion end */
AdcHandle.Init.LowPowerAutoWait = DISABLE; /* Auto-delayed conversion feature disabled */
AdcHandle.Init.ContinuousConvMode = DISABLE; /* Continuous mode disabled to have only 1 conversion at each conversion trig */
AdcHandle.Init.NbrOfConversion = 1; /* Parameter discarded because sequencer is disabled */
AdcHandle.Init.DiscontinuousConvMode = DISABLE; /* Parameter discarded because sequencer is disabled */
AdcHandle.Init.NbrOfDiscConversion = 1; /* Parameter discarded because sequencer is disabled */
AdcHandle.Init.ExternalTrigConv = ADC_SOFTWARE_START; /* Software start to trig the 1st conversion manually, without external event */
AdcHandle.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; /* Parameter discarded because software trigger chosen */
AdcHandle.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DR; /* Regular Conversion data stored in DR register only */
AdcHandle.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN; /* DR register is overwritten with the last conversion result in case of overrun */
AdcHandle.Init.OversamplingMode = DISABLE; /* No oversampling */
if (HAL_ADC_Init(&AdcHandle) != HAL_OK)
{
/* ADC initialization Error */
Error_Handler();
}
/*##-2- Configure ADC regular channel ######################################*/
sConfig.Channel = ADCx_CHANNEL; /* Sampled channel number */
sConfig.Rank = ADC_REGULAR_RANK_1; /* Rank of sampled channel number ADCx_CHANNEL */
sConfig.SamplingTime = ADC_SAMPLETIME_8CYCLES_5; /* Sampling time (number of clock cycles unit) */
sConfig.SingleDiff = ADC_SINGLE_ENDED; /* Single-ended input channel */
sConfig.OffsetNumber = ADC_OFFSET_NONE; /* No offset subtraction */
sConfig.Offset = 0; /* Parameter discarded because offset correction is disabled */
if (HAL_ADC_ConfigChannel(&AdcHandle, &sConfig) != HAL_OK)
{
/* Channel Configuration Error */
Error_Handler();
}
/* Run the ADC calibration in single-ended mode */
if (HAL_ADCEx_Calibration_Start(&AdcHandle, ADC_CALIB_OFFSET, ADC_SINGLE_ENDED) != HAL_OK)
{
/* Calibration Error */
Error_Handler();
}
/*##-3- Start the conversion process #######################################*/
if (HAL_ADC_Start(&AdcHandle) != HAL_OK)
{
/* Start Conversation Error */
Error_Handler();
}
/*##-4- Wait for the end of conversion #####################################*/
/* For simplicity reasons, this example is just waiting till the end of the
conversion, but application may perform other tasks while conversion
operation is ongoing. */
if (HAL_ADC_PollForConversion(&AdcHandle, 10) != HAL_OK)
{
/* End Of Conversion flag not set on time */
Error_Handler();
}
else
{
/* ADC conversion completed */
/*##-5- Get the converted value of regular channel ########################*/
uhADCxConvertedValue = HAL_ADC_GetValue(&AdcHandle);
}
Found it on "Repository\STM32Cube_FW_H7_V1.10.0\Projects\NUCLEO-H743ZI\Examples\ADC\ADC_RegularConversion_Polling"
2022-04-20 08:59 AM
I have compared with my code, it is pretty much what I currently have, but unfortunately it does not work.
I'm playing with clock settings, but still cannot get it to work.
2022-04-20 05:16 PM
Unfortunately, I do not have that MCU.
Can you screen capture your CubeMX settings?
ALso, try on other pins as well.
2022-04-20 07:01 PM
2022-04-21 07:20 AM
I also tried with PA3 pin (ADC1 channel 8), same result as with channel 7.
I tried same ADC configuration on H723 and F411 and there were no problems with those.
2022-04-21 07:57 AM
I pretty much copied the settings of ADC and set clock to same values and used an internal oscilator.
I have noticed that function ADC_Enable returns an error (HAL_ERROR) - timeout occours.
But if I again call HAL_ADC_Start_IT it returns HAL_OK. I'm not sure what is happening here. Also interrupts are comming and HAL_ADC_GetValue is still returning value 0.
2022-05-11 06:41 AM
Below code needs to be added after inicialization of adc in order for adc to work:
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWREx_EnableVddA();