2020-12-03 3:18 AM
This does not happen with STM32CubeIDE 1.4, but I need to use 1.5 for various reasons. The computer doesn't have and can't have an internet connection.
I've downloaded the file en.stm32cubef4_v1-25-0.zip, AND en.patch_cubef4.zip (this is V1.25.2 according to ST, and the one that doesn't work).
I've also downloaded the file STM32CubeF4-master.zip from the ST repo on Github, but STM32CubeIDE doesn't recognize it as a firmware package.
I've googled this problem for days, but can't seem to find an answer. I've also searched the forums, and can only find similar problems with CubeProgrammerMX, but none are marked as solved.
2020-12-07 5:49 AM
I wonder why no one is answering?
2021-06-11 8:41 AM