2025-03-11 8:14 AM
Hello,
I have some issues with STM32CubeIDE and the use of a middleware in a classroom. The goal is to teach the students to use the software and the LoRaWAN middleware however with have some issues where STM32CubeIDE ask for st.com account for .ioc compilation and code generation (even if we had the LoRaWAN middleware installed by hand).
How can we have a working configuration for a classroom without asking all students to create an account ?
Bests regards,
Lounès DUPUIS-DABAJI
2025-04-10 7:37 AM
Hello @Raserber
First I want to thank you for posting.
In fact to download firmware packages to create projects, you need to connect to your st account in STM32CubeIDE.
Check the STM32CubeIDE user manual UM2609 section 1.2.3 STM32CubeIDE user authentication for more details.
BR,
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-12 4:17 AM - edited 2025-04-12 4:20 AM
So kind of ST, annoying everyone in the planet yet they keep ignoring their users.
This might work.
If you already have a working IDE, skip the following.
> Login in one PC, compile the project, let it it download everything.
Assuming a Windows system, copy the folder C:\Users\_username_\STM32Cube\Repository and paste it in the others.
As far as I know, you can omit the big zip files, only the copy the subfolders.