cancel
Showing results for 
Search instead for 
Did you mean: 

Problem configuring ADC4 inputs with STM32CubeMx 6.13.0

JVERN.18
Associate III

Hello,

I have a problem with configuring some GPIO as input for the ADC4:

While they appear to be available in the documentation (and in the pop-up window associated with GPIO), the choice is grayed out in the tab associated with ADC4.


I'm using STM32CubeMx version 6.13.0 (but it's the same with previous versions).


Is this a bug or did I forget something?

Sincerely,

Jean-Louis

img1.pngimg2.pngimg3.png

1 ACCEPTED SOLUTION

Accepted Solutions
Souhaib MAZHOUD
ST Employee

Hello @JVERN.18 

As mentioned in the screenshot below, channel IN22 is only available if the sequencer is not fully configurable. Therefore, you can configure ADC4_IN22 as well.

SouhaibMAZHOUD_0-1732718481962.png

 

Thx,

Souhaib

 

View solution in original post

4 REPLIES 4
Souhaib MAZHOUD
ST Employee

Hello @JVERN.18 

Could you provide the name of the MCU that result this issue!

 

mƎALLEm
ST Employee

Hello,

Do you mean for STM32U5F7, the the channels from 15 to Channel 23 + VDAC_OUT1 are grayed out?

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Souhaib MAZHOUD
ST Employee

Hello @JVERN.18 

As mentioned in the screenshot below, channel IN22 is only available if the sequencer is not fully configurable. Therefore, you can configure ADC4_IN22 as well.

SouhaibMAZHOUD_0-1732718481962.png

 

Thx,

Souhaib

 

JVERN.18
Associate III

Thank you for your response.

I didn't stay on the checkboxes long enough to see the message.

Furthermore, I don't really understand why in one case we can have access to all the inputs and why in the other this is not the case (and I did not find a super clear answer in the documentation), but I realize that it is like that!

Thanks again.

Jean-Louis