cancel
Showing results for 
Search instead for 
Did you mean: 

Package error when importing examples of NUCLEO-U031R8

Torris-Yin
Associate II

The MCU of NUCLEO-U031R8 is LQFP64. But if I import the example of NUCLEO-U031R8, STM32CubeMX shows it as UFBGA64.

TorrisYin_0-1734259967063.png

 

1 ACCEPTED SOLUTION

Accepted Solutions

Hi @Torris-Yin ,

I see the contradiction now.

For the selected project: the mounted device is STM32U031R8Tx (LQFP64 package).

ImenD_0-1734360849671.png

But, when you open the project, it is mentioned STM32U031R8Ix (which is UFBGA64 package).

ImenD_2-1734361440867.png

Thank you for rising this up.

I escalated this issue to our CubeMX team (via internal ticket number: 198841)

(PS: Internal ticket number is only for ST reference, not accessible outside of ST)

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

3 REPLIES 3
Imen.D
ST Employee

Hello @Torris-Yin ,

The STM32U031R8T6 MCU is an LQFP64 package, and STM32U031R8I6 is an UFBGA64 package.

In your case, you are using the example with STM32U031R8Ix which is an UFBGA64 package.

ImenD_0-1734337756271.png

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

Hello, @Imen.D 

I am using the example of NUCLEO-U031R8, which is STM32U031R8T6. I attached a video of my operation.

Thanks. 

TorrisYin_0-1734357791909.png

 

Hi @Torris-Yin ,

I see the contradiction now.

For the selected project: the mounted device is STM32U031R8Tx (LQFP64 package).

ImenD_0-1734360849671.png

But, when you open the project, it is mentioned STM32U031R8Ix (which is UFBGA64 package).

ImenD_2-1734361440867.png

Thank you for rising this up.

I escalated this issue to our CubeMX team (via internal ticket number: 198841)

(PS: Internal ticket number is only for ST reference, not accessible outside of ST)

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen