cancel
Showing results for 
Search instead for 
Did you mean: 

Is there anything wrong in using standard libraries in embedded system programming ?

Bastien LS
Associate III

I am currently working on the STM35U5 family using STM32CubeMX, and I see that none of the code generated is using the standard libraries.

Why is that? Should I avoid using standard libraries in my application code ?

1 ACCEPTED SOLUTION

Accepted Solutions
Danish1
Lead III

Which standard libraries do you mean?

Standard libraries were written with the assumption of a large computer and things like file-systems, console I/O. And probably an operator on-hand to get things going again if/when they fail.

Even with a "clever" linker, they use a lot of memory; not so much of a problem on stm32u5, but prohibitive on some of the smaller stm32l0

Unless Stm32CubeMx needs what a specific standard library was written to provide (e.g. string-handling, file I/O) then there's no point having it.

One specific point for embedded system programming, many people do not like dynamic memory allocation (malloc & free; new & delete) and instead prefer to statically allocate every variable that will be needed (except those on the stack). This avoids the risk of running-out-of-memory at run-time, either because of too much instantaneous demand for variables or that memory has become fragmented over the run.

And C string handling needs care to prevent buffer overruns - original K&R C libraries were not written with such risks foremost in the programmers' minds.

As long as you know and understand the risks, you are the skilled engineer best-placed to decide which libraries to use with your code.

Hope this helps,

Danish

View solution in original post

1 REPLY 1
Danish1
Lead III

Which standard libraries do you mean?

Standard libraries were written with the assumption of a large computer and things like file-systems, console I/O. And probably an operator on-hand to get things going again if/when they fail.

Even with a "clever" linker, they use a lot of memory; not so much of a problem on stm32u5, but prohibitive on some of the smaller stm32l0

Unless Stm32CubeMx needs what a specific standard library was written to provide (e.g. string-handling, file I/O) then there's no point having it.

One specific point for embedded system programming, many people do not like dynamic memory allocation (malloc & free; new & delete) and instead prefer to statically allocate every variable that will be needed (except those on the stack). This avoids the risk of running-out-of-memory at run-time, either because of too much instantaneous demand for variables or that memory has become fragmented over the run.

And C string handling needs care to prevent buffer overruns - original K&R C libraries were not written with such risks foremost in the programmers' minds.

As long as you know and understand the risks, you are the skilled engineer best-placed to decide which libraries to use with your code.

Hope this helps,

Danish