2021-05-12 06:50 AM
Hello, when testing the SDcard on SDIO 1-bit interface , we see a big problem here:
when card in slot, cpu stall in MX_SDMMC2_SD_Init() , on debug can see: card info sector count, block size etc. read seem ok, but then waiting for response -- forever. (timeout -1)
SDclk set to 200/(4*2) MHz, 1-bit mode; tried different things: cache on/off, clk faster/slow, extra cap close to card holder, different cards, core volt.scale 0/1; now i am out of ideas, why it is not working. looked also H7A3 errata, but there i see no problem with SD .
Stall/wait is here, in init :
while (!__HAL_SD_GET_FLAG(hsd, SDMMC_FLAG_RXOVERR | SDMMC_FLAG_DCRCFAIL | SDMMC_FLAG_DTIMEOUT | SDMMC_FLAG_DATAEND))
so: what is wrong? do i something wrong? or is something missing?
Solved! Go to Solution.
2021-05-20 04:09 AM
Thx for your response.
AN5200 was on my list...and i use STM32CubeIDE, Version: 1.6.1, cube 6.2.1-RC2 ;
with update to actual version and after "right" setting of pins got it working now.
Read-speed about 3,4 MB/s , 1bit mode;
setting: 200Mhz clk, div 2 (gives clk/4 -> 50MHz SDHC standard; pins CMD+D0 : pullup, speed medium ("FAST" on H7A3 ).
With same setting also running on STM32H753 now.
and on my small STM32F411 board, 100MHz clk, div 0 (!) , 4 bit mode, all pins: pullup and high speed, get about 8MB/s read from microSD. =)
(speed is effective speed, including f_read() and without DMA , tested with 10KB block reading)
just what STM could do better: when using cube -> in RCC LSE clock initial setting : LSE drive -> high drive cap. This would save a lot of people wondering, why cpu not always start or stall .
and here, for SDMMC , setting for pins : pullups and medium/fast speed setting.
regards
Alfred
2021-05-19 10:17 AM
Hello @AScha.3 and welcome to the STM32 Community,
I added the adequate topics to your question in order to increase its chance to be reviewed by our experts.
Which CubeMX and CubeH7 package version are you using ?
If possible to share your ioc file or the source code to check more this behavior.
Have a look at this AN5200 "Getting started with STM32H7 Series SDMMC host controller", which contains typical examples and it may help you on the SDMMC configuration.
Imen
2021-05-20 04:09 AM
Thx for your response.
AN5200 was on my list...and i use STM32CubeIDE, Version: 1.6.1, cube 6.2.1-RC2 ;
with update to actual version and after "right" setting of pins got it working now.
Read-speed about 3,4 MB/s , 1bit mode;
setting: 200Mhz clk, div 2 (gives clk/4 -> 50MHz SDHC standard; pins CMD+D0 : pullup, speed medium ("FAST" on H7A3 ).
With same setting also running on STM32H753 now.
and on my small STM32F411 board, 100MHz clk, div 0 (!) , 4 bit mode, all pins: pullup and high speed, get about 8MB/s read from microSD. =)
(speed is effective speed, including f_read() and without DMA , tested with 10KB block reading)
just what STM could do better: when using cube -> in RCC LSE clock initial setting : LSE drive -> high drive cap. This would save a lot of people wondering, why cpu not always start or stall .
and here, for SDMMC , setting for pins : pullups and medium/fast speed setting.
regards
Alfred
2021-05-20 04:16 AM
Hi @AScha.3 ,
Really glad to know you overcame this problem :)
Thank you for all the details you provided. I will let our teams know about your suggestion.
Thank you once more for your contribution.
Imen