Skip to main content
AVoel.1
Associate III
December 14, 2024
Question

Pretty Printers for STL containers on MacOS? (Can't view STL container contents in the debugger)

  • December 14, 2024
  • 0 replies
  • 546 views

I could swear this used to work, but out of the box I do not seem to be able to display the contents of STL containers on my Mac using STM32CubeIDE. A little googling reveals that this has to do with having the Python pretty printers for GDB installed properly, so it seems that that is not the case on my system. And it seems that this should be handled in the standard install of STM32CubeIDE. But it does not seem to be.

I am running STMCubeIDE 1.17, but I didn't install it from scratch, I upgraded using the built in upgrade facility. I'm running MacOS 15, but I'm fairly certain this did not work using MacOS 14 either.

Questions:

  1. Is this the experience of other STM32CubeIDE users on MacOS?
  2. If so, does anyone have instructions on the proper install of the pretty printers to get it working. I can probably piece it together from other internet posts, but that could potentially be a time consuming and frustrating process.
This topic has been closed for replies.