![Screenshot 2024-12-13 085847.png Screenshot 2024-12-13 085847.png](https://community.st.com/t5/image/serverpage/image-id/96103i91B41B7BCED5F598/image-size/large/is-moderation-mode/true?v=v2&px=999)
my english is not good,i use chatgpt to help me to generate this post.
Hello,
I am working on a project with the STM32H750 microcontroller using CubeMX-generated code and HAL library. My system clock configuration is as follows:
- HCLK: 240 MHz
- PCLK2: Configured via D2PPRE2
I encountered an issue related to HAL_RCC_GetPCLK2Freq() and UART configuration. Here is the detailed description:
Issue Description
- When D2PPRE2 (APB2 prescaler) is set to no division (DIV1), HAL_RCC_GetPCLK2Freq() correctly returns 240 MHz, and the UART works as expected at the configured baud rate (e.g., 115200).
- However, when D2PPRE2 is configured to divide by 2 (DIV2):
- HAL_RCC_GetPCLK2Freq() still returns 240 MHz (unaffected by the prescaler).
- The UART actual baud rate becomes half of the configured value (e.g., if I configure 115200, the actual baud rate is 57600).
- This indicates that the prescaler is applied to PCLK2 in hardware, but the HAL function does not account for it correctly.
Steps to Reproduce
- Configure D2PPRE2 to DIV2 in CubeMX.
- Initialize UART with a baud rate of 115200 using HAL_UART_Init().
- Measure the actual UART baud rate using an oscilloscope or logic analyzer.
STM32CubeIDE Version: 1.17.0