‎2019-01-07 02:02 PM
in CubeMX V5.01 release note, it says:
• The TrueSTUDIO™ IDE is not supported.
Is this only for this version release or for future as well?
‎2019-01-07 02:12 PM
I thought they bought Atollic to have an IDE, not kill it, so at some point it is likely to be supported in some form. Perhaps they are working on the IDE to provide a more universal/flexible import method, and thus reduce the regression work rather than keeping expanding it?
A winning commercial strategy is to be able to import the projects from ALL your primary competitors, but hey what do I know...
‎2019-01-07 03:04 PM
I couldn't beleive it, so I just created a new project with CubeMX 5.0.1 and exported into TrueStudio without any problems.
:flushed_face:
‎2019-01-07 03:07 PM
Perhaps they mean the HAL libraries, a lot of the Atollic example/template project stuff was jettisoned a while back.