2018-03-30 9:03 AM
Hello,
I have a device based on STM32F1 series that's using the USB CDC interface. TrueSTUDIO project is generated with STM32CubeMX. Everything is working fine except one last thing: Setting the serial number string from code. I can set the serial number string from STM32CubeMX or by overriding the define in Code
#define USBD_SERIALNUMBER_STRING_FS '00000000001A'�?But I need the string to be unique per device, so using the MCU UID to generate an unique number would be the best solution. Generated parts are:
[...]
USBD_DescriptorsTypeDef FS_Desc =
{
 USBD_FS_DeviceDescriptor
, USBD_FS_LangIDStrDescriptor
, USBD_FS_ManufacturerStrDescriptor
, USBD_FS_ProductStrDescriptor
, USBD_FS_SerialStrDescriptor
, USBD_FS_ConfigStrDescriptor
, USBD_FS_InterfaceStrDescriptor
};
[...]
uint8_t * USBD_FS_SerialStrDescriptor(USBD_SpeedTypeDef speed, uint16_t *length)
{
 if(speed == USBD_SPEED_HIGH)
 {
 USBD_GetString((uint8_t *)USBD_SERIALNUMBER_STRING_FS, USBD_StrDesc, length);
 }
 else
 {
 USBD_GetString((uint8_t *)USBD_SERIALNUMBER_STRING_FS, USBD_StrDesc, length);
 }
 return USBD_StrDesc;
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
[...]�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?I see no way to insert user code into theUSBD_FS_SerialStrDescriptor function, since there is no USER CODE field. What is the
STM32CubeMX
way to use a serial number from the UID? Am I missing something here? #usb-cdc #usb-device #stm32cubemx2018-04-09 9:28 AM
Anyone? Someone from ST? There must be a intended way, to use the UID as USB serial.
2018-04-09 12:11 PM
The compiler builds the code it is presented.
Just add your own code to convert the part's Unique ID into a string and provide that as a descriptor. The goal with CubeMX is that you don't keep pressing the 'rebuild button' over and over, rather that you keep your working project in it's own safe tree, and sandbox experimental/incremental changes which you can then merge into the main tree.
>>There must be a intended way, to use the UID as USB serial.
I wouldn't assume that anyone is really thinking this out beyond the horizon of their own task list.
2018-04-09 3:46 PM
It's funny that all the USB Device example projects in the Cube repository use the device UID as USB serial, and yet the code generator is incapable of providing such solution.
You could simply copy the usbd_desc.c file from e.g. {F1 repo}/Projects/STM3210E_EVAL/Applications/USB_Device/CDC_Standalone/Src to your project and call USBD_Init() with VCP_Desc parameter instead of FS_Desc.
2018-04-10 1:19 AM
Turvey.Clive.002
 So, CubeMX was not designed to regenerate the code once the project has been generated? I doubt that, it would make it useless, since requirements are changing in the development process. But that's not the point, I don't expect that CubeMX generates me a proper function to use the UID as serial, but I do expect that I can override the default behaviour of using the define as serial. As I mentioned, there is noUSER CODEarea in usbd_desc.c and especially not in theUSBD_FS_SerialStrDescriptor function which is responsible to build the serial portion of FS_Desc. If I make any changes to the settings in CubeMX and regenerate the project while 'Keep User Code when re-generating' is set, I'm loosing everything that is not in an
USER CODE area.
Kupper.Benedek
 Unfortunatelythese examples are not for CubeMX. If I just copy the whole file, it would be just replaced on the next re-generate from CubeMX.2018-04-10 3:47 AM
Unfortunately these examples are not for CubeMX. If I just copy the whole file, it would be just replaced on the next re-generate from CubeMX.
It's only true if you put it in the same directory as the generated file.
2018-04-10 4:10 AM
Of course, but I don't see the point. If I move my own
usbd_desc.c or just rename it, I would need to include it at least from usb_device.c which is generated or edit the project's includes which are generated. I mean almost every other generated function from CubeMX provides USER CODE areas and I had no problems at all to implement everything I need there. It seems
usbd_desc.c kinda does not fit the pattern.
2019-01-08 12:39 AM
It is also entertaining to see that that the two cases of the speed check if does the same :)