2017-04-08 02:03 AM
Hi. I'm using STM32CubeMX V4.20.1 and System Workbench for STM32(SW4STM32) now.
Actually I use CubeMX plugin for SW4STM32.
the problem is...when I click 'Generate Code' after changing the gpios or timers or any changes, project properties(more exactly Optimization) that I was set before changed after load the modified project.I'll show you example pictures.I think that is CubeMX V4.20.1's one of problem#optimization #propertied #cubemx #sw4stm322017-04-09 01:53 PM
Hi Jisu Kim,
I will check this issue and report it internally if confirmed.
We will keep you informed of any updates.
Imen
2017-04-09 05:47 PM
Thank you!
2017-04-12 08:06 AM
hello
Kim.Jisu
,I understand your point however, I can't reproduce it. When I change the optimization level in SW4STM32/Eclipse, the paremeter value is kept even if the project is reloaded.
On my point of view, the parameter optimization level is a parameter from Eclipse that is not given by CubeMX.
I wonder what arethe versions of your openSTM32IDE and ARM Compiler for MCU in Eclipse:
I have these versions :
If you don't have the version 1.1.201701200843, please upgrade it and keep me informed if you still have the issue or not.
BR. Eric
2017-04-12 10:36 AM
Hello
Joly.Jeanne
!Thank you for replying. My OpenSTM32IDE and ARM Compiler for MCU version is like below.
- OpenSTM32IDE : 1.0.201703061529
- ARM Compiler for MCU : 1.2.201703061592
I did reinstall CubeMX v4.1 but it didn't work too. So I installed CubeMX v4.0 and it fixed my problem.
well, I don't know what was problem, but now goes well. That's weird...
here's my eclipse installation details.
Thank you!
(and below link is my process? progress? when I did install CubeMX 4.1)
2017-07-10 05:29 AM
I'm having the exact same issue.
CubeMX 4.21.0
OpenSTM32 IDE 1.13.1.201701200843
ARM Compiler for MCU 1.13.1.201701200843