2022-10-15 09:22 AM
I am using stm32f407zg board with DP83848 ethernet PHY chip. CubeMX generates code with LWIP for FreeRTOS. App used to answer ping successfully when it starts with connected eth cable only and stops after its reconnecting. After some investigation i have noticed some suspicious place in code(see below). After adding "_IT" postfix it started to work, so looks like cube used wrong handler to stop/start ETH periphery(see lines 7 and 30). So my question is: is it a CubeMX bug or i just missed some delails?
Here is a cycle from ethernet_link_thread entry in ethernetif.c file:
for(;;)
{
PHYLinkState = DP83848_GetLinkState(&DP83848);
if(netif_is_link_up(netif) && (PHYLinkState <= DP83848_STATUS_LINK_DOWN))
{
HAL_ETH_Stop_IT(&heth); //Here we stop ETH
netif_set_down(netif);
netif_set_link_down(netif);
}
else if(!netif_is_link_up(netif) && (PHYLinkState > DP83848_STATUS_LINK_DOWN))
{
switch (PHYLinkState)
{
case DP83848_STATUS_100MBITS_FULLDUPLEX:
duplex = ETH_FULLDUPLEX_MODE;
speed = ETH_SPEED_100M;
linkchanged = 1;
break;
...
}
if(linkchanged)
{
/* Get MAC Config MAC */
HAL_ETH_GetMACConfig(&heth, &MACConf);
MACConf.DuplexMode = duplex;
MACConf.Speed = speed;
HAL_ETH_SetMACConfig(&heth, &MACConf);
HAL_ETH_Start(&heth); // HERE IS A POSSIBLE BUG by using wrong handle to start ETH
netif_set_up(netif);
netif_set_link_up(netif);
}
}
Solved! Go to Solution.
2024-08-12 07:23 AM - edited 2024-08-12 07:23 AM
Can someone at ST listen to @Piranha and fix these bugs?