2017-08-02 02:42 AM
I have a clean slate CubeMX project on a STM32F401C-Discovery board. I have set up the onboard Cirrus audio DAC, and send a hard-coded test signal to it via DMA-driven I2S. I can hear the sound, but it is at wrong frequency.
The 2kHz test signal, and the i2s-3 is set to 48kHz samplerate, but depending on how I configure the PLL, I hear 122Hz, 180Hz or 244Hz audio. I have confirmed with a logic analyzer that the I2S protocol runs too slow. The only things I have changed from the CubeMX generated template project is:In the source code, I only initialize the DAC and enable the DMA. No other changes to the generated source are done.
The three configurations I tried with:
PLLM=4 gives a I2S WS (frame clock) of 2.93kHz, and the 2kHz audio is at 122Hz:With PLLM=6, I see a WS of 4.4kHz, and audio at 184Hz:
And with PLLM=8, WS is at 5.859kHz, and the audio at 244Hz:
CubeMX is version 4.21.0, F4-firmware package is version 1.16.0
Going through the STM32F401 reference manual and device registers hasn't yet given me a clue where CubeMX generates the bug.
Suggestions (and CubeMX bugfixes) much appreciated
kalle
#cubemx #i2s #frequencySolved! Go to Solution.
2017-08-03 12:59 AM
waclawek.jan wrote:
PS. What's written on the chip?
That's it! Thanks for the tip.
While the board is clearly labeled 'STM32F401C-DISCO', the chip on it is, in fact a STM32F411VET6U.
So in Cube's jargon, I have a 'STM32F411E-DISCO' board. Perhaps it said so on the package, but that is lost in time.
(Now looking on my Nucleo boards, the board label is on a sticker. But seems the Nucleo boards don't seem to have a default value under the sticker... Anyways, I can't recall this Discovery board ever having had a sticker on it.)
Almost besides the point now, but as an explanation for the problems above: it seems the F411 has separate PLL_M divisors for I2S and the rest of the system. Using the correct chip in CubeMX solves the issue - the audio comes out at 2kHz now.
Thanks for the help. This was a learning experience
kalle
2017-08-02 03:15 AM
Output the I2S and main clock to MCO to check.
Read out and post the content of relevant RCC and SPI/I2S registers.
JW
2017-08-02 04:45 AM
Hi
Raiskila.Kalle
,What is your target I2S bitrate (the frequency atwhichyou are willing to send the datato the DAC)?
Jae
2017-08-02 06:02 AM
But you still can measure the bitclock (I2S_CK) can't you. With the above setting it should be exactly 3MHz.
JW
2017-08-02 06:38 AM
RCC:
SPI3:
Did I miss any relevant ones?
This is taken after MX_I2S_Init() has finished, but before transmission. The only odd thing I can find is the I2SE (enabled) bit is zero here,
but if I interrupt the processor when it has started streaming, even that bit is set (I2SCFGR=0x0e01).
This is the configuration from above where PLL_M=4
(Edit: I need to find a more high-powered analyzer to check the clocks via MCO. Will do this as soon as possible)
2017-08-02 06:55 AM
Hi,
I'm targeting 48kHz samplerate, with 2*32 bits per sample (actually 16 bits data on a 32 bit frame). So bitrate is 3.072Mbps.
The test signal is 2kHz sine wave sampled at 48kHz. A standard 1kHz sine was nolonger recognizable as a sine wave in the audio output. At least with these low quality speakers
2017-08-02 07:21 AM
Well, I expected my post will make you think and do the analysis (read: homework) yourself... :-)
There's no RCC_PLLCR in RM0368, I take it you meant RCC_CR.
If I calculate it correctly, you have:
- both PLLs and HSE ON (and also HSI ON but that does not matter except for a miniscule increase in consumption)
- PLLM = 4 => PLL input is 2MHz (if the Xtal is 8MHz indeed)
- PLLN=144 (that does not match the M=4 picture from above)
- PLLP = 1 => /4 => (together with HPRE =0 i.e. AHB not divided) SYSCLK = 8/4*144/4 = 72MHz
- PLLQ = 6
- I2S clock is PLLI2S
- PLLI2SN = 192
- PLLI2SR = 2 => I2SClock = 8/4*192/2=192MHz
Is this what you wanted? Can you confirm it with outputting the I2SPLL onto MCO2 and observing it using the LA?
SPI_I2SPR.MCKOE = 1 i.e. MCK is enabled
I2SDIV = 8 and ODD = 0 => MCK frequency is 192MHz/(2*8+0) = 12MHz Can you confirm it?
JW
2017-08-02 07:50 AM
Yes. That is how I calculated it too
The PLL_N=144 is correct, and matches what CubeMX says. I was toying around with values to see what changes, so it didn't match the above picture anymore. Sorry for the confusion, my bad. Same for the PLLI2SCLK, was 96MHz in the above pictures, in the register capture case 192MHz. (It did not have any impact on the I2S WS or audio)I'll have to measure those clocks, soonest (I currently have only the smallest Saleae at hand, 12Msps max)
But what puzzles me is how the I2S speed varies with PLL_M, as the PLLI2SCLK is kept a constant 96MHz in each of the three cases above (as well as with PLLI2SCLK is 192MHz - I2S speed varies with PLL_M only). This is surely not intended behaviour? But perhaps the clocks will give a hint at what is happening here too.Thanks for your input,
kalle
2017-08-02 07:58 AM
And oh yes, the HSE crystal is labeled 8MHz, and this is what CubeMX sets it to when I load the board's default config. So that hopefully is not the problem here
2017-08-02 08:39 AM
Yes, the I2S bitclock is measurable. With the above register settings, it is 187.5 kHz which is 2*32*Fs (here the measured Fs(i.e. I2S_WS)=2.93kHz).
So it seems the SPI/I2S hw block is getting some strange input clock?