2025-03-12 10:40 PM
I make a new product with NetXDuo for STM32H743.
But, it is included error code in RTE_Components.h
RTE_Components.h (A project)
/* USER CODE END Header */
/* Define to prevent recursive inclusion -------------------------------------*/
#ifndef __RTE_COMPONENTS_H__
#define __RTE_COMPONENTS_H__
/* Defines ------------------------------------------------------------------*/
/* STMicroelectronics.X-CUBE-AZRTOS-H7.3.3.0 */
#define FILEX_ENABLED
#define FX_SD_INTERFACE
NX_ETH_INTERFACE_ENABLED
#define LAN8742
#define THREADX_ENABLED
#define TRACEX_SUPPORT_ENABLED
#define NETXDUO_ENABLED
#endif /* __RTE_COMPONENTS_H__ */
RTE_Components.h (B project)
/* Define to prevent recursive inclusion -------------------------------------*/
#ifndef __RTE_COMPONENTS_H__
#define __RTE_COMPONENTS_H__
/* Defines ------------------------------------------------------------------*/
/* STMicroelectronics.X-CUBE-AZRTOS-H7.3.3.0 */
#define USBXDEVICE_ENABLED
#define UX_DEVICE_CONTROLLERS_ENABLED
#define UX_DEVICE_CDC_ACM
#define FILEX_ENABLED
#define FX_SD_INTERFACE
NX_ETH_INTERFACE_ENABLED
#define LAN8742
#define THREADX_ENABLED
#define TRACEX_SUPPORT_ENABLED
#define NETXDUO_ENABLED
#endif /* __RTE_COMPONENTS_H__ */
it is missing '#define' statement for 'NX_ETH_INTERFACE_ENABLED'.
Fortunately, the error does not occur becasue the RTE_Components.h file is not built.
2025-03-14 3:33 AM
Hello @JongOk Baek
First let me thank you for posting.
Could you please provide your IOC so that I can check your configuration and investigate further the issue?
I will be waiting for your feedback.
THX
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-03-14 4:28 AM
2025-03-14 5:22 AM
Hello @JongOk Baek
Thanks for your contribution.
Issue has been raised to dev team for fix .
Internal ticket number :197472
BR,
Ghofrane
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.