cancel
Showing results for 
Search instead for 
Did you mean: 

CubeMX does not run - just shows start screen, then stops

Viktro
Associate II

CubeMX shows the light blue start screen, and stops without any message!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!

8 REPLIES 8

Welcome to the forum.

What version of CubeMX ?

Running on what platform? and version?

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228

 

CubeMX 16.3,    Windows 11 Pro, AMD Ryzen 5 3600 6-Core Processor 3.60 GHz

Ozone
Lead III

That's not much information.

On a proper OS, you could start CubeMX from a console and watch for error messages.

And since it is Eclipse-based, the usual log files are created in a subdirectory.
Check those for further information.

Is the CubeMX (standalone) Eclipse based?

Yes

No log file

So did you try starting it from a command-line?

Hello @Viktro 

Try to launch the installation using cmd and please provide your .log.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen