2022-10-27 1:21 PM
Solved! Go to Solution.
2022-10-31 9:38 AM
Hello @gbm
I was able to reproduce the behavior concerning the default settings.
This problem is raised internally to be reviewed. I'll keep you posted with the updates.
Internal ticket number: 137942 (This is an internal tracking number and is not accessible or usable by customers).
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-10-30 11:48 PM
Hello @gbm
Thank you for rising this up.
I added my colleague @Semer CHERNI from CubeMx team, as he can help you on your issue.
Regarding point2: please refer to this post MX_DMA_Init order in the main.c file generated by STM32CubeMX, How to fix?
Imen
2022-10-31 2:58 AM
After removing FunctionListSort line, the correct order is set and the generated project becomes usable but it is still not possible to change the order of init functions in AdvancedSettings.
So, the problem is MOSTLY solved. Thanks.
Anyway, the MCU package and maybe CubeMX still need fixing.
2022-10-31 9:38 AM
Hello @gbm
I was able to reproduce the behavior concerning the default settings.
This problem is raised internally to be reviewed. I'll keep you posted with the updates.
Internal ticket number: 137942 (This is an internal tracking number and is not accessible or usable by customers).
Semer.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.