cancel
Showing results for 
Search instead for 
Did you mean: 

Can G491 OPAMP6 be connected to ADC3?

yjsbd
Associate II

0693W000008xSTkQAM.pngIn RM0440, STM32G491 is Category 4.

Therefore OPAMP6 can be connected to ADC3 refer to RM0440 21.4.4(ADC Connectivity)

But I cannot find check option for OPAMP6 in ADC3 setting.

Is it unavailable? or not implemented yet?

4 REPLIES 4
yjsbd
Associate II

in "stm32g4xx_ll_adc.h" OPAMP6 is available in ADC3.

It seems just cubemx bug

Khouloud ZEMMELI
ST Employee

Hello @yjsbd​ 

Thank you for your feedback,

I have checked on my side and yes, you're totally right, there's an issue in CubeMX regarding the OPAMP6 connectivity with ADC3, a VOPAMP6 Channel is missed under ADC3.

Thanks for raising this issue to our attention :) it will be fixed.

Khouloud

Hello @yjsbd​ ,

I'm back again to inform you that issue is now fixed, you can use the latest CubeMX version availabel on site :)

Khouloud

HDaji.1
Senior

Is there a good tutorial on how to use OPAMP and ADC on G4 board?