Browse
STMicroelectronics Community
FAQs
Sign In
Product forums
STM32 MCUs
STM32 MCUs products
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
STM32 MCUs Other solutions
STM32 MPUs
STM32 MPUs products
STM32 MPUs Boards and hardware tools
STM32 MPUs Software development tools
STM32 MPUs Embedded software
STM32 MPUs Solutions
MEMS and sensors
MEMS (sensors)
Imaging (sensors)
Automotive & Transportation
Microcontrollers
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
yjsbd
Associate II
since
2019-03-12
2023-06-14
User statistics
5
Posts
0
Solutions
0
Kudos given
0
Kudos received
STMicroelectronics Community
About yjsbd
Options
Report User
User Activity
Posts
Replies
Can G491 OPAMP6 be connected to ADC3?
2021-03-19
In RM0440, STM32G491 is Category 4.Therefore OPAMP6 can be connected to ADC3 refer to RM0440 21.4.4(ADC Connectivity)But I cannot find check option for OPAMP6 in ADC3 setting.Is it unavailable? or not implemented yet?
USBH_MSC_ClassRequest looks buggy when using USB host MSC class
2019-03-12
in usbh_msc.cif(status == USBH_OK) { MSC_Handle->max_lun = (MSC_Handle->max_lun > MAX_SUPPORTED_LUN)? MAX_SUPPORTED_LUN : (uint8_t )(MSC_Handle->max_lun) + 1U; USBH_UsrLog ("Number of supported LUN: %lu", (int32_t)(MSC_Handle->max_lun)); ...
Re: Can G491 OPAMP6 be connected to ADC3?
2021-03-19
in "stm32g4xx_ll_adc.h" OPAMP6 is available in ADC3.It seems just cubemx bug
Re: USBH_MSC_ClassRequest looks buggy when using USB host MSC class
2019-03-12
I'm using STM32F4 firmware V1.24
Re: USBH_MSC_ClassRequest looks buggy when using USB host MSC class
2019-03-12
Some USB flash drive failed to get read inquiry.After I modified processing getmaxlun, it works fine